I want to upgrade my project from compiler tools v6 to v8. The project includes DSP/Bios v5.42.
When compiling I get many errors on s62 file generated by XDCTools (v3.50), like "Invalid constant specification".
Does it mean that there is an incompatibility between compiler tools v8 and DSP/Bios v5.42 and/or XDCTools v3.50 ?
Should I upgrade to DSP/Bios v6 ?
Pascal