Part Number: AM6442
Hi ,
We have an am6442 board and getting error "** Unrecognized filesystem type **"when trying to boot from emmc.
Please find the log below
**********************************************************
ERROR
=> setenv mmcdev 0
=> setenv bootpart 0:1
=> saveenv
Saving Environment to MMC... Writing to MMC(0)... OK
=> boot
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
** Unrecognized filesystem type **
Bad Linux ARM64 Image magic!
*************************************************************
Please find below the output of partitions and mmc commands
***********************************************************************
=> mmc list
sdhci@fa10000: 0 (eMMC)
sdhci@fa00000: 1
=> mmc part
Partition Map for MMC device 0 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000800 0x0766ffde ""
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
guid: 9f74cc9b-7a4e-1940-a4eb-b6cb4e806673
=> printenv partitions
partitions=name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
=> print
arch=arm
args_all=setenv optargs earlycon=ns16550a,mmio32,0x02800000 ${mtdparts}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=am64x
board_name=am64x_gpevm
boot=mmc
boot_fdt=try
bootargs=console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern) root=PARTUUID=9f74cc9b-7a4e-1940-a4eb-b6cb4e806673 rw rootfstype=ext4 rootwait
bootcmd=run findfdt; run envboot; run init_${boot}; run get_kern_${boot}; run get_fdt_${boot}; run run_kern
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootm_size=0x10000000
bootpart=0:1
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyS2,115200n8
cpu=armv8
dtboaddr=0x89000000
envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
ethaddr=f4:84:4c:f9:5e:3a
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=fdef5e38
fdtfile=k3-am642-evm.dtb
findfdt=if test $board_name = am64x_gpevm; then setenv fdtfile k3-am642-evm.dtb; fi; if test $board_name = am64x_skevm; then setenv fdtfile k3-am642-sk.dtb; fi;if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
finduuid=part uuid mmc ${bootpart} uuid
get_fdt_mmc=load mmc ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
get_fit_mmc=load mmc ${bootpart} ${addr_fit} ${bootdir}/${name_fit}
get_kern_mmc=load mmc ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
get_overlay_mmc=fdt address ${fdtaddr};fdt resize 0x100000;for overlay in $name_overlays;do;load mmc ${bootpart} ${dtboaddr} ${bootdir}/${overlay} && fdt apply ${dtboaddr};done;
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
init_mmc=run args_all args_mmc
ipaddr=192.168.2.25
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadbootscript=load mmc ${mmcdev} ${loadaddr} boot.scr
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mmcboot=mmc dev ${mmcdev}; devnum=${mmcdev}; setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then run args_mmc; if test ${boot_fit} -eq 1; then run run_fit; else run mmcloados;fi;fi;fi;
mmcdev=0
mmcloados=if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
mtdids=nor0=fc40000.spi.0
mtdparts=mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern)
name_kern=Image
optargs=earlycon=ns16550a,mmio32,0x02800000 mtdparts=fc40000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern)
partitions=name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rd_spec=-
rdaddr=0x88080000
run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
scriptaddr=0x80000000
serial#=0000000000000000
serverip=192.168.2.44
soc=k3
stderr=serial@2800000
stdin=serial@2800000
stdout=serial@2800000
uuid=9f74cc9b-7a4e-1940-a4eb-b6cb4e806673
vendor=ti
Environment size: 3719/131068 bytes
***************************************************************************************************************************
Any help is appreciated.NEed to solve this as soon as possible.
Thanks and Regards,
Radhika