This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI Driver for Dm6446



Hi,

We are using DM6446 EVM for Interfacing an external SPI device. We configured the SPI registers accordingly (For 4 Wire communication). We are using the SPI driver as a pluggable module. We had refered the SPI peripheral user manual (SPRUE32A.pdf) and also we have taken care for the silicon errata also. But even after the proper configuration of registers, we are not able to see any communication between DM6446 EVM (Which is acting as a MASTER)  and external SPI device (which is acting as Slave). We can't see the SPI_CLK signal also. Can any one help us on this regard.