Part Number: PROCESSOR-SDK-AM335X
Hi
after an update of my host OS to dosfstools the sd-carts I create with my host OS won't boot.
This is because the fat partition starts different, I think. Below I have two images in a compressed file, one working and one not working
I did do a manual hex compair of both images, the start of it is different as shown below. I like to know if the differences in the fat partition fail to get u-boot loaded
Below the start of the working fat partition: 0xEB, 0x58, 0x90, 0x6D, 0x6B, 0x66, 0x73, 0x2E, 0x66, 0x61, 0x74, 0x00, 0x02, 0x01, 0x20, 0x00, 0x02, 0x00, 0x00, 0x00, 0x00, 0xF8, 0x00, 0x00, 0x3E, 0x00, 0xF2, 0x00, 0x00, 0x08, 0x00, 0x00, >>0x00, 0x20<<, 0x03, 0x00, 0x28, 0x06, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x02, 0x00, 0x00, 0x00, 0x01, 0x00, 0x06, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x01, 0x29, >>0xD3, 0x83, 0xCB, 0xC5<<, 0x62, 0x6F, 0x6F, 0x74, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x46, 0x41, 0x54, 0x33, 0x32, 0x20, 0x20, 0x20, 0x0E, 0x1F, 0xBE, 0x77, 0x7C, 0xAC, 0x22, 0xC0, 0x74, 0x0B, 0x56, 0xB4, 0x0E, 0xBB, 0x07, 0x00, 0xCD, 0x10, 0x5E, 0xEB, 0xF0, 0x32, 0xE4, 0xCD, 0x16, 0xCD, 0x19, 0xEB, 0xFE, 0x54, 0x68, 0x69, 0x73, 0x20, 0x69, 0x73, 0x20, 0x6E, 0x6F, 0x74, 0x20, 0x61, 0x20, 0x62, 0x6F, 0x6F, 0x74, 0x61, 0x62, 0x6C, 0x65, 0x20, 0x64, 0x69, 0x73, 0x6B, 0x2E, 0x20, 0x20, 0x50, 0x6C, 0x65, 0x61, 0x73, 0x65, 0x20, 0x69, 0x6E, 0x73, 0x65, 0x72, 0x74, 0x20, 0x61, 0x20, 0x62, 0x6F, 0x6F, 0x74, 0x61, 0x62, 0x6C, 0x65, 0x20, 0x66, 0x6C, 0x6F, 0x70, 0x70, 0x79, 0x20, 0x61, 0x6E, 0x64, 0x0D, 0x0A, 0x70, 0x72, 0x65, 0x73, 0x73, 0x20, 0x61, 0x6E, 0x79, 0x20, 0x6B, 0x65, 0x79, 0x20, 0x74, 0x6F, 0x20, 0x74, 0x72, 0x79, 0x20, 0x61, 0x67, 0x61, 0x69, 0x6E below the start of the not working partition: 0xEB, 0x58, 0x90, 0x6D, 0x6B, 0x66, 0x73, 0x2E, 0x66, 0x61, 0x74, 0x00, 0x02, 0x01, 0x20, 0x00, 0x02, 0x00, 0x00, 0x00, 0x00, 0xF8, 0x00, 0x00, 0x3E, 0x00, 0xF2, 0x00, 0x00, 0x08, 0x00, 0x00,>> 0xF2, 0x1F,<< 0x03, 0x00, 0x28, 0x06, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x02, 0x00, 0x00, 0x00, 0x01, 0x00, 0x06, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x01, 0x29,>> 0x52, 0x23, 0x2B, 0x09<<, 0x62, 0x6F, 0x6F, 0x74, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x20, 0x46, 0x41, 0x54, 0x33, 0x32, 0x20, 0x20, 0x20, 0x0E, 0x1F, 0xBE, 0x77, 0x7C, 0xAC, 0x22, 0xC0, 0x74, 0x0B, 0x56, 0xB4, 0x0E, 0xBB, 0x07, 0x00, 0xCD, 0x10, 0x5E, 0xEB, 0xF0, 0x32, 0xE4, 0xCD, 0x16, 0xCD, 0x19, 0xEB, 0xFE, 0x54, 0x68, 0x69, 0x73, 0x20, 0x69, 0x73, 0x20, 0x6E, 0x6F, 0x74, 0x20, 0x61, 0x20, 0x62, 0x6F, 0x6F, 0x74, 0x61, 0x62, 0x6C, 0x65, 0x20, 0x64, 0x69, 0x73, 0x6B, 0x2E, 0x20, 0x20, 0x50, 0x6C, 0x65, 0x61, 0x73, 0x65, 0x20, 0x69, 0x6E, 0x73, 0x65, 0x72, 0x74, 0x20, 0x61, 0x20, 0x62, 0x6F, 0x6F, 0x74, 0x61, 0x62, 0x6C, 0x65, 0x20, 0x66, 0x6C, 0x6F, 0x70, 0x70, 0x79, 0x20, 0x61, 0x6E, 0x64, 0x0D, 0x0A, 0x70, 0x72, 0x65, 0x73, 0x73, 0x20, 0x61, 0x6E, 0x79, 0x20, 0x6B, 0x65, 0x79, 0x20, 0x74, 0x6F, 0x20, 0x74, 0x72, 0x79, 0x20, 0x61, 0x67, 0x61, 0x69, 0x6E differences in start of partition marked with >><<