Part Number: TDA4VM-Q1
We would like to inquire about abnormal operation of TDA. The TDA4 did not supply power and did not operate.
However, it is measured as 0.6V at the RGMII6_RXC port (W26).
The I/O port connected with TDA4 is the I2C interface of MCU.
If the current from the I2C port flows back into the TDA4, Can power be measured on I/O ports on the TDA4?