Other Parts Discussed in Thread: OMAP-L138
I have a few questions regarding the LCD controller on the OMAP-L138. This does not seem clear to me from the datasheet or LCDC user's guide.
When does the DMA start relative to the start of frame generation with respect to the external LCD control signals? I’m interested in both cases of from LCD_EN and from frame to frame when double buffering is used. i.e. with DMA0 and DMA1 mode. When does the second DMA start relative to the EOF bit set of the first when performing continuous frame updates?
I would also like to estimate the time from the last EOF0/1 interrupt bit being set in a frame to the start of DMA for the next frame. I know this depends on system composition so I’m mainly interested in LCDC synchronous timing events, enough to determine a minimum time if only the LCDC had access to the DDR.
Thanks,
David