This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSSK3358: How to boot linux kernel using rootfs on memory?

Part Number: TMDSSK3358


To anyone concerned

Hello,
I'm using TMDSSK3358 board and trying to boot up Linux Kernel through USB port or ethernet only.
That means I have to put the rootfs on memory, using a ramdisk or the zImage.

I have two questions here, and first let me show what I tried.

Now I have the SDK ver.7.3. I tryed to follow the explanation on the URL shown below.(6.1.15. Program the eMMC on Beaglebone Black)
downloads.ti.com/.../Program_the_eMMC_on_Beaglebone_Black.html
But, it seems out of date and not matches my usecase exactly.

For example, there is no file named arago-tiny-image-am335x-evm.tar.xz in <Processor-SDK>/filesystem,
so I have to use tisdk-tiny-image-am335x-evm.tar.xz as the rootfs.

As setting menuconfig, though the html's image was different with that the SDK showed, I just tryed enable the Items mentioned.
Then I made zImage using the following command.
make ARCH=arm CROSS_COMPILE=<mypath>/arm-none-linux-gnueabihf- zImage.

I inputted an empty SD card into TMDSSK3358, connected the host with USB and ethernet, then switched the board on.
When u-boot is loaded, I stopped autoboot and typed the following script to start kernel.

=> run findfdt
=> run init_console
=> dhcp
=> run netloadfdt
=> setenv bootargs console=ttyO0,115200
=> bootz ${loadaddr} - ${fdtaddr}

The result is that the kernel was not started correctly.
The following is the console message.

-----------------------------------------------------------------------
=> bootz ${loadaddr} - ${fdtaddr}
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df22000, end 8df34d95 ... OK

Starting kernel ...
-----------------------------------------------------------------------

My first question is:
How can I do the same thing with what 6.1.15 said using a TMDSSK3358 board and the SDK ver.7.3 ?

My second question is:
If I want to start linux kernel with ramdisk (commands showed below),
what should I do with TMDSSK3358 board and the SDK ver.7.3?

Commands:
=> run findfdt
=> run init_console
=> dhcp
=> run netloadfdt
=> tftp ${rdaddr} ramdisk.gz
=> run ramargs
=> bootz ${loadaddr} ${rdaddr} ${fdtaddr}