Part Number: TDA4VM
Hello,
There are several problems when I use DCC to tuning images:
1. After changing the exposure time in manual AE mode, the image does not change. Is that normal?
2. When I calibrate the AWB and modify the "tuning radius", the Cb-Cr plot scheme does not change, as shown in below. And I can't find the "Red/Green/Blue scaler for flourescent" mentioned in the AWB guide.

There are no change after I update AWB calibration and tuning parameters to the camera.
3. I copied the bin and XML files generated by DCC to the directory: /opt/vision_apps/dcc/<sensor_name>/<wdr_mode> , ran the "run_app_single_cam.sh" and pressed the u command, the image did not change. The whole process was done according to the manual: https://www.ti.com/lit/pdf/spracu7.
The camera I used is AR0820, and the version of SDK is 7.03. Please give me some help on these problems, thanks.