Part Number: AM5729
Hi,
I have a problem with TIDL Importer from the AM57XX SDK. Im trying to import an object detection model trained on Caffe-Jacinto. The model seems to be exported right because when it comes to calibration I can see this output
Target: number label value xmin ymin xmax ymax Target: 0.00 1.00 0.42 -0.05 0.22 0.99 0.86
So this means that the model detects the object on the image. But when I'm using this exported model on the BeagleBone AI in the SSD example, it doesn't detect anything. This same happens on the model on which my model was fine-tuned. I've used this model for fine-tuning.
The problem is not with the confidence threshold, because even when I set it to 1 doesn't change anything. So how should the model be imported to run on BB AI?