Part Number: AM6442
Our customer is concerned about the power connection when MMC0 is not used.
For VDD_MMC0 and VDD_DLL_MMC0, the datasheet describes that if MMC0 is not used, each of these balls must be connected to the same power source as VDD_CORE.
VDD_MMC0 and VDD_DLL_MMC0 are 0.85V inputs, but if the LP873364 is used, the power source to VDD_CORE is 0.75V.

If MMC0 is not used, is the above power connection correct?
Best regards,
Daisuke