This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi-
For various corporate reasons, I am trying to get CCS x.x running on Windows 10 (64-bit) using XDS510 USB (Plus) emulator.
- Traget DSP Model: TMS320VC5416
Please recommend a development environment.
1. Last CCS version for TMS320VC5416 ?
2. Last Windows version for TMS320VC5416?
3. Flashburn version or replacement program compatible with CCS last version(num. '1') ?
4. Is it possible to use XDS510USB(num '1', '2') ?
Thank you.
Have a good day.
Hi Byeong,
The last CCS supports C5416 is 6.2.0.00050 (Sept. 14, 2016).
There is a built in USB interface to on-board JTAG controller (J201) and a external JTAG connector (J7) on the C5416 DSK. The XDS510USB should work with the CCS 6.2.0. You may need to download the Spectrum Digital C55x package.
Best rgards,
Ming