HI,
I've customize my rootfs using yocto with the help of training series of TI. I've booted my board using this customised images.
Now im running dsp application by loading using mpmcl command.
But as soon as i start running application using "mpmcl run dsp0" within 2-3 min my entire system getting crashed and i'm getting the error log as follows.
please help me to reslove this.
[ 254.591343] UBIFS error (ubi0:0 pid 310): ubifs_read_node: bad node type (221 but expected 1)
[ 254.616922] UBIFS error (ubi0:0 pid 310): ubifs_read_node: bad node at LEB 10 2:157080, LEB mapping status 1
[ 254.648268] Not a node, first 24 bytes:
[ 254.648277] 00000000: dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd d d dd dd dd dd dd ........................
[ 254.699530] CPU: 0 PID: 310 Comm: sshd Tainted: G O 4.19.94-gb e5389fd85 #1
[ 254.723987] Hardware name: Keystone
[ 254.734399] Backtrace:
[ 254.741705] [<c020ca30>] (dump_backtrace) from [<c020cd68>] (show_stack+0x18/ 0x1c)
[ 254.764342] r7:00000066 r6:600f0013 r5:00000000 r4:c1243e9c
[ 254.781261] [<c020cd50>] (show_stack) from [<c09ea340>] (dump_stack+0x9c/0xb0 )
[ 254.802863] [<c09ea2a4>] (dump_stack) from [<c0492164>] (ubifs_read_node+0x24 c/0x250)
[ 254.826277] r7:00000066 r6:ffffffea r5:00026598 r4:cfd9c000
[ 254.843200] [<c0491f18>] (ubifs_read_node) from [<c04adcbc>] (ubifs_tnc_read_ node+0xd0/0xd4)
[ 254.868436] r10:00000018 r9:00000000 r8:cfd9c0cc r7:cfd9c000 r6:ed102000 r5: 00000001
[ 254.891848] r4:cfdb8980
[ 254.899407] [<c04adbec>] (ubifs_tnc_read_node) from [<c0495260>] (ubifs_tnc_l ocate.part.2+0xc8/0x1e8)
[ 254.926982] r7:ed279ce0 r6:00000001 r5:c1204c48 r4:cfd9c000
[ 254.943902] [<c0495198>] (ubifs_tnc_locate.part.2) from [<c049539c>] (ubifs_t nc_locate+0x1c/0x24)
[ 254.970437] r10:00000014 r9:00000a7e r8:ed102000 r7:c1204c48 r6:eff3c50c r5: 00021d0c
[ 254.993848] r4:ee601000
[ 255.001406] [<c0495380>] (ubifs_tnc_locate) from [<c0487aec>] (do_readpage+0x 10c/0x3cc)
[ 255.025342] [<c04879e0>] (do_readpage) from [<c0488d58>] (ubifs_readpage+0x54 /0x518)
[ 255.048498] r10:ee601000 r9:00000013 r8:00000014 r7:00000000 r6:cfd9c000 r5: eff3c50c
[ 255.071910] r4:c1204c48
[ 255.079472] [<c0488d04>] (ubifs_readpage) from [<c02e1908>] (filemap_fault+0x 39c/0x6a8)
[ 255.103408] r10:00080001 r9:ed6ce300 r8:00000014 r7:00000000 r6:ee6010fc r5: 006200ca
[ 255.126821] r4:eff3c50c
[ 255.134379] [<c02e156c>] (filemap_fault) from [<c030f010>] (__do_fault+0x54/0 x150)
[ 255.157014] r10:c02df94c r9:b6f41000 r8:ed279e30 r7:00000d73 r6:ed24a138 r5: ed279e30
[ 255.180425] r4:c1204c48
[ 255.187983] [<c030efbc>] (__do_fault) from [<c031452c>] (handle_mm_fault+0x8b 4/0xde8)
[ 255.211397] r7:00000d73 r6:0000001f r5:00000040 r4:c1204c48
[ 255.228314] [<c0313c78>] (handle_mm_fault) from [<c0214dd4>] (do_page_fault+0 x124/0x33c)
[ 255.252509] r10:cfe4b83c r9:ed24a138 r8:80000207 r7:b6f41164 r6:cfe4b800 r5: ed032f40
[ 255.275920] r4:ed279fb0
[ 255.283476] [<c0214cb0>] (do_page_fault) from [<c021529c>] (do_PrefetchAbort+ 0x48/0xc4)
[ 255.307412] r10:00000004 r9:00000003 r8:ed279fb0 r7:b6f41164 r6:c1209cdc r5: 00000207
[ 255.330824] r4:c1204c48
[ 255.338380] [<c0215254>] (do_PrefetchAbort) from [<c0201f60>] (ret_from_excep tion+0x0/0x20)
[ 255.363353] Exception stack(0xed279fb0 to 0xed279ff8)
[ 255.378448] 9fa0: 00595428 00000000 00000 136 00000001
[ 255.402903] 9fc0: b6f5e524 b6f5e060 00595428 00000001 0057bc24 00000003 00000 004 0059a578
[ 255.427356] 9fe0: bed861c0 bed86120 b6f422f8 b6f41164 20070010 ffffffff
[ 255.447131] r9:00000003 r8:30c5387d r7:30c5387d r6:ffffffff r5:20070010 r4:b 6f41164
[ 255.482911] UBIFS error (ubi0:0 pid 310): do_readpage: cannot read page 20 of inode 2686, error -22
[ 255.517636] UBIFS error (ubi0:0 pid 310): ubifs_read_node: bad node type (221 but expected 1)
[ 255.544445] UBIFS error (ubi0:0 pid 310): ubifs_read_node: bad node at LEB 10 2:157080, LEB mapping status 1
[ 255.574389] Not a node, first 24 bytes:
[ 255.574397] 00000000: dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd d d dd dd dd dd dd ........................
[ 255.625540] CPU: 0 PID: 310 Comm: sshd Tainted: G O 4.19.94-gb e5389fd85 #1
[ 255.649997] Hardware name: Keystone
[ 255.660411] Backtrace:
[ 255.667717] [<c020ca30>] (dump_backtrace) from [<c020cd68>] (show_stack+0x18/ 0x1c)
[ 255.690353] r7:00000066 r6:600f0013 r5:00000000 r4:c1243e9c
[ 255.707272] [<c020cd50>] (show_stack) from [<c09ea340>] (dump_stack+0x9c/0xb0 )
[ 255.728871] [<c09ea2a4>] (dump_stack) from [<c0492164>] (ubifs_read_node+0x24 c/0x250)
[ 255.752287] r7:00000066 r6:ffffffea r5:00026598 r4:cfd9c000
[ 255.769210] [<c0491f18>] (ubifs_read_node) from [<c04adcbc>] (ubifs_tnc_read_ node+0xd0/0xd4)
[ 255.794445] r10:00000018 r9:00000000 r8:cfd9c0cc r7:cfd9c000 r6:ed102000 r5: 00000001
[ 255.817859] r4:cfdb8980
[ 255.825419] [<c04adbec>] (ubifs_tnc_read_node) from [<c0495260>] (ubifs_tnc_l ocate.part.2+0xc8/0x1e8)
[ 255.852993] r7:ed279ce0 r6:00000001 r5:c1204c48 r4:cfd9c000
[ 255.869913] [<c0495198>] (ubifs_tnc_locate.part.2) from [<c049539c>] (ubifs_t nc_locate+0x1c/0x24)
[ 255.896448] r10:00000014 r9:00000a7e r8:ed102000 r7:c1204c48 r6:eff3c50c r5: 00021d0c
[ 255.919859] r4:ee601000
[ 255.927418] [<c0495380>] (ubifs_tnc_locate) from [<c0487aec>] (do_readpage+0x 10c/0x3cc)
[ 255.951356] [<c04879e0>] (do_readpage) from [<c0488d58>] (ubifs_readpage+0x54 /0x518)
[ 255.974512] r10:ee601000 r9:00000014 r8:00000014 r7:00000000 r6:cfd9c000 r5: eff3c50c
[ 255.997924] r4:c1204c48
[ 256.005484] [<c0488d04>] (ubifs_readpage) from [<c02e16d8>] (filemap_fault+0x 16c/0x6a8)
[ 256.029419] r10:00080001 r9:ed6ce300 r8:00000014 r7:00000000 r6:ee6010fc r5: ee601000
[ 256.052831] r4:eff3c50c
[ 256.060390] [<c02e156c>] (filemap_fault) from [<c030f010>] (__do_fault+0x54/0 x150)
[ 256.083025] r10:c02df94c r9:b6f41000 r8:ed279e30 r7:00000d73 r6:ed24a138 r5: ed279e30
[ 256.106436] r4:c1204c48
[ 256.113994] [<c030efbc>] (__do_fault) from [<c031452c>] (handle_mm_fault+0x8b 4/0xde8)
[ 256.137409] r7:00000d73 r6:0000001f r5:00000040 r4:c1204c48
[ 256.154326] [<c0313c78>] (handle_mm_fault) from [<c0214dd4>] (do_page_fault+0 x124/0x33c)
[ 256.178520] r10:cfe4b83c r9:ed24a138 r8:80000207 r7:b6f41164 r6:cfe4b800 r5: ed032f40
[ 256.201932] r4:ed279fb0
[ 256.209488] [<c0214cb0>] (do_page_fault) from [<c021529c>] (do_PrefetchAbort+ 0x48/0xc4)
[ 256.233422] r10:00000004 r9:00000003 r8:ed279fb0 r7:b6f41164 r6:c1209cdc r5: 00000207
[ 256.256833] r4:c1204c48
[ 256.264390] [<c0215254>] (do_PrefetchAbort) from [<c0201f60>] (ret_from_excep tion+0x0/0x20)
[ 256.289362] Exception stack(0xed279fb0 to 0xed279ff8)
[ 256.304457] 9fa0: 00595428 00000000 00000 136 00000001
[ 256.328911] 9fc0: b6f5e524 b6f5e060 00595428 00000001 0057bc24 00000003 00000 004 0059a578
[ 256.353364] 9fe0: bed861c0 bed86120 b6f422f8 b6f41164 20070010 ffffffff
[ 256.373139] r9:00000003 r8:30c5387d r7:30c5387d r6:ffffffff r5:20070010 r4:b 6f41164
[ 256.401552] UBIFS error (ubi0:0 pid 310): do_readpage: cannot read page 20 of inode 2686, error -22
[ 256.442408] UBIFS error (ubi0:0 pid 970): ubifs_read_node: bad node type (221 but expected 9)
[ 256.469272] UBIFS error (ubi0:0 pid 970): ubifs_read_node: bad node at LEB 13 0:119424, LEB mapping status 1
[ 256.499262] Not a node, first 24 bytes:
[ 256.499269] 00000000: dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd d d dd dd dd dd dd ........................
[ 256.550408] CPU: 0 PID: 970 Comm: kworker/u2:0 Tainted: G O 4. 19.94-gbe5389fd85 #1
[ 256.576946] Hardware name: Keystone
[ 256.587359] Backtrace:
[ 256.594665] [<c020ca30>] (dump_backtrace) from [<c020cd68>] (show_stack+0x18/ 0x1c)
[ 256.617303] r7:00000082 r6:600f0013 r5:00000000 r4:c1243e9c
[ 256.634223] [<c020cd50>] (show_stack) from [<c09ea340>] (dump_stack+0x9c/0xb0 )
[ 256.655822] [<c09ea2a4>] (dump_stack) from [<c0492164>] (ubifs_read_node+0x24 c/0x250)
[ 256.679238] r7:00000082 r6:ffffffea r5:0001d280 r4:cfd9c000
[ 256.696160] [<c0491f18>] (ubifs_read_node) from [<c04ad878>] (ubifs_load_znod e+0x94/0x408)
[ 256.720876] r10:0001d280 r9:00000082 r8:cfda4c68 r7:ed121cc0 r6:000000bc r5: ed2d2200
[ 256.744289] r4:cfd9c000
[ 256.751848] [<c04ad7e4>] (ubifs_load_znode) from [<c0495060>] (ubifs_lookup_l evel0+0xc8/0x200)
[ 256.777605] r10:c1204c48 r9:00000000 r8:ed27ddc0 r7:00000000 r6:00000100 r5: cfd9c000
[ 256.801017] r4:ed27dcf8
[ 256.808577] [<c0494f98>] (ubifs_lookup_level0) from [<c04951f8>] (ubifs_tnc_l ocate.part.2+0x60/0x1e8)
[ 256.836154] r10:00000018 r9:00000000 r8:cfd9c0cc r7:ed27ddc0 r6:00000000 r5: c1204c48
[ 256.859565] r4:cfd9c000
[ 256.867124] [<c0495198>] (ubifs_tnc_locate.part.2) from [<c0495b14>] (ubifs_t nc_lookup_nm+0x40/0x140)
[ 256.894701] r10:ed27ddc0 r9:00000944 r8:cfe26200 r7:ed27dda4 r6:cfd9c000 r5: 70888ae6
[ 256.918113] r4:c1204c48
[ 256.925673] [<c0495ad4>] (ubifs_tnc_lookup_nm) from [<c04b3db0>] (ubifs_xattr _get+0xc4/0x210)
[ 256.951168] r10:ed27de54 r9:00000944 r8:ee65eb40 r7:cfe26200 r6:cfd9c000 r5: 70888ae6
[ 256.974579] r4:c1204c48
[ 256.982139] [<c04b3cec>] (ubifs_xattr_get) from [<c04b3f24>] (xattr_get+0x28/ 0x2c)
[ 257.004775] r10:cfdf69b0 r9:c1204c48 r8:c120c578 r7:ed27de54 r6:edbf6110 r5: c04b3efc
[ 257.028187] r4:ee65eb40
[ 257.035748] [<c04b3efc>] (xattr_get) from [<c036c7ac>] (__vfs_getxattr+0x60/0 x70)
[ 257.058122] r5:c04b3efc r4:ee65eb40
[ 257.068802] [<c036c74c>] (__vfs_getxattr) from [<c04dff60>] (get_vfs_caps_fro m_disk+0x6c/0x180)
[ 257.094817] r7:ed2d2100 r6:c1204c48 r5:ed27dea8 r4:cfdf6980
[ 257.111733] [<c04dfef4>] (get_vfs_caps_from_disk) from [<c04e0210>] (cap_bprm _set_creds+0x19c/0x540)
[ 257.139048] r8:c0c01c8c r7:ed2d2100 r6:00000001 r5:cfdf6200 r4:cfdf6980
[ 257.159086] [<c04e0074>] (cap_bprm_set_creds) from [<c034bd28>] (prepare_binp rm+0x138/0x18c)
[ 257.184322] r10:00000001 r9:00000000 r8:ed2a4d04 r7:00000000 r6:ee65eb40 r5: c1204c48
[ 257.207733] r4:ed2d2100
[ 257.215290] [<c034bbf0>] (prepare_binprm) from [<c034cfa0>] (__do_execve_file +0x478/0x738)
[ 257.240005] r8:ed2a4d04 r7:00000000 r6:ed2d2100 r5:ed452000 r4:c1204c48
[ 257.260041] [<c034cb28>] (__do_execve_file) from [<c034d2c8>] (do_execve+0x30 /0x38)
[ 257.282935] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5: ed2a4d40
[ 257.306346] r4:cfdf6200
[ 257.313905] [<c034d298>] (do_execve) from [<c0235134>] (call_usermodehelper_e xec_async+0x198/0x1c8)
[ 257.340963] [<c0234f9c>] (call_usermodehelper_exec_async) from [<c02010d8>] ( ret_from_fork+0x14/0x3c)
[ 257.368536] Exception stack(0xed27dfb0 to 0xed27dff8)
[ 257.383631] dfa0: 00000000 00000000 00000 000 00000000
[ 257.408085] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000 000 00000000
[ 257.432538] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 257.452311] r7:00000000 r6:00000000 r5:c0234f9c r4:ed2a4d40
[ 257.481575] Invalid argument reading file caps for /lib/systemd/systemd-cored ump
[ 257.513270] Core dump to |/lib/systemd/systemd-coredump 310 0 0 7 1638956255 4294967295 k2g-evm sshd pipe failed
[ 261.915946] UBIFS error (ubi0:0 pid 308): ubifs_read_node: bad node type (221 but expected 1)
[ 261.941654] UBIFS error (ubi0:0 pid 308): ubifs_read_node: bad node at LEB 10 2:157080, LEB mapping status 1
[ 261.972704] Not a node, first 24 bytes:
[ 261.972712] 00000000: dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd d d dd dd dd dd dd ........................
[ 262.023961] CPU: 0 PID: 308 Comm: sshd Tainted: G O 4.19.94-gb e5389fd85 #1
[ 262.048418] Hardware name: Keystone
[ 262.058831] Backtrace:
[ 262.066136] [<c020ca30>] (dump_backtrace) from [<c020cd68>] (show_stack+0x18/ 0x1c)
[ 262.088773] r7:00000066 r6:600f0013 r5:00000000 r4:c1243e9c
[ 262.105693] [<c020cd50>] (show_stack) from [<c09ea340>] (dump_stack+0x9c/0xb0 )
[ 262.127293] [<c09ea2a4>] (dump_stack) from [<c0492164>] (ubifs_read_node+0x24 c/0x250)
[ 262.150710] r7:00000066 r6:ffffffea r5:00026598 r4:cfd9c000
[ 262.167630] [<c0491f18>] (ubifs_read_node) from [<c04adcbc>] (ubifs_tnc_read_ node+0xd0/0xd4)
[ 262.192867] r10:00000018 r9:00000000 r8:cfd9c0cc r7:cfd9c000 r6:ed102000 r5: 00000001
[ 262.216280] r4:cfdb8980
[ 262.223841] [<c04adbec>] (ubifs_tnc_read_node) from [<c0495260>] (ubifs_tnc_l ocate.part.2+0xc8/0x1e8)
[ 262.251417] r7:ed249ce0 r6:00000001 r5:c1204c48 r4:cfd9c000
[ 262.268336] [<c0495198>] (ubifs_tnc_locate.part.2) from [<c049539c>] (ubifs_t nc_locate+0x1c/0x24)
[ 262.294871] r10:00000014 r9:00000a7e r8:ed102000 r7:c1204c48 r6:eff3c50c r5: 00021d0c
[ 262.318282] r4:ee601000
[ 262.325841] [<c0495380>] (ubifs_tnc_locate) from [<c0487aec>] (do_readpage+0x 10c/0x3cc)
[ 262.349779] [<c04879e0>] (do_readpage) from [<c0488d58>] (ubifs_readpage+0x54 /0x518)
[ 262.372934] r10:ee601000 r9:00000014 r8:00000014 r7:ed208368 r6:cfd9c000 r5: eff3c50c
[ 262.396346] r4:c1204c48
[ 262.403907] [<c0488d04>] (ubifs_readpage) from [<c02e16d8>] (filemap_fault+0x 16c/0x6a8)
[ 262.427844] r10:c02df94c r9:ed208300 r8:00000014 r7:ed208368 r6:80000022 r5: ee601000
[ 262.451256] r4:eff3c50c
[ 262.458815] [<c02e156c>] (filemap_fault) from [<c030f010>] (__do_fault+0x54/0 x150)
[ 262.481450] r10:c02df94c r9:b6f6b000 r8:ed249e30 r7:00000d73 r6:ed238138 r5: ed249e30
[ 262.504862] r4:c1204c48
[ 262.512418] [<c030efbc>] (__do_fault) from [<c031452c>] (handle_mm_fault+0x8b 4/0xde8)
[ 262.535834] r7:00000d73 r6:00000018 r5:00000040 r4:c1204c48
[ 262.552751] [<c0313c78>] (handle_mm_fault) from [<c0214dd4>] (do_page_fault+0 x124/0x33c)
[ 262.576946] r10:cfe4b43c r9:ed238138 r8:80000207 r7:b6f6b164 r6:cfe4b400 r5: ed033600
[ 262.600358] r4:ed249fb0
[ 262.607914] [<c0214cb0>] (do_page_fault) from [<c021529c>] (do_PrefetchAbort+ 0x48/0xc4)
[ 262.631850] r10:00000004 r9:00000003 r8:ed249fb0 r7:b6f6b164 r6:c1209cdc r5: 00000207
[ 262.655262] r4:c1204c48
[ 262.662819] [<c0215254>] (do_PrefetchAbort) from [<c0201f60>] (ret_from_excep tion+0x0/0x20)
[ 262.687792] Exception stack(0xed249fb0 to 0xed249ff8)
[ 262.702887] 9fa0: 004acdf8 00000000 00000 134 00000001
[ 262.727342] 9fc0: b6f88524 b6f88060 004acdf8 00000001 00493c24 00000003 00000 004 004b0f18
[ 262.751795] 9fe0: be9221c0 be922120 b6f6c2f8 b6f6b164 20070010 ffffffff
[ 262.771570] r9:00000003 r8:30c5387d r7:30c5387d r6:ffffffff r5:20070010 r4:b 6f6b164
[ 262.801621] UBIFS error (ubi0:0 pid 308): do_readpage: cannot read page 20 of inode 2686, error -22
[ 262.840427] UBIFS error (ubi0:0 pid 972): ubifs_read_node: bad node type (221 but expected 9)
[ 262.866994] UBIFS error (ubi0:0 pid 972): ubifs_read_node: bad node at LEB 13 0:119424, LEB mapping status 1
[ 262.897078] Not a node, first 24 bytes:
[ 262.897085] 00000000: dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd dd d d dd dd dd dd dd ........................
[ 262.948213] CPU: 0 PID: 972 Comm: kworker/u2:0 Tainted: G O 4. 19.94-gbe5389fd85 #1
[ 262.974751] Hardware name: Keystone
[ 262.985164] Backtrace:
[ 262.992470] [<c020ca30>] (dump_backtrace) from [<c020cd68>] (show_stack+0x18/ 0x1c)
[ 263.015108] r7:00000082 r6:600f0013 r5:00000000 r4:c1243e9c
[ 263.032026] [<c020cd50>] (show_stack) from [<c09ea340>] (dump_stack+0x9c/0xb0 )
[ 263.053627] [<c09ea2a4>] (dump_stack) from [<c0492164>] (ubifs_read_node+0x24 c/0x250)
[ 263.077042] r7:00000082 r6:ffffffea r5:0001d280 r4:cfd9c000
[ 263.093963] [<c0491f18>] (ubifs_read_node) from [<c04ad878>] (ubifs_load_znod e+0x94/0x408)
[ 263.118680] r10:0001d280 r9:00000082 r8:cfda4c68 r7:ed121d80 r6:000000bc r5: ed2d2300
[ 263.142093] r4:cfd9c000
[ 263.149652] [<c04ad7e4>] (ubifs_load_znode) from [<c0495060>] (ubifs_lookup_l evel0+0xc8/0x200)
[ 263.175409] r10:c1204c48 r9:00000000 r8:ed2addc0 r7:00000000 r6:00000106 r5: cfd9c000
[ 263.198821] r4:ed2adcf8
[ 263.206380] [<c0494f98>] (ubifs_lookup_level0) from [<c04951f8>] (ubifs_tnc_l ocate.part.2+0x60/0x1e8)
[ 263.233955] r10:00000018 r9:00000000 r8:cfd9c0cc r7:ed2addc0 r6:00000000 r5: c1204c48
[ 263.257366] r4:cfd9c000
[ 263.264925] [<c0495198>] (ubifs_tnc_locate.part.2) from [<c0495b14>] (ubifs_t nc_lookup_nm+0x40/0x140)
[ 263.292501] r10:ed2addc0 r9:00000944 r8:cfe26000 r7:ed2adda4 r6:cfd9c000 r5: 70888ae6
[ 263.315912] r4:c1204c48
[ 263.323471] [<c0495ad4>] (ubifs_tnc_lookup_nm) from [<c04b3db0>] (ubifs_xattr _get+0xc4/0x210)
[ 263.348966] r10:ed2ade54 r9:00000944 r8:ee65eb40 r7:cfe26000 r6:cfd9c000 r5: 70888ae6
[ 263.372378] r4:c1204c48
[ 263.379935] [<c04b3cec>] (ubifs_xattr_get) from [<c04b3f24>] (xattr_get+0x28/ 0x2c)
[ 263.402570] r10:cfdf69b0 r9:c1204c48 r8:c120c578 r7:ed2ade54 r6:edbf6110 r5: c04b3efc
[ 263.425980] r4:ee65eb40
[ 263.433542] [<c04b3efc>] (xattr_get) from [<c036c7ac>] (__vfs_getxattr+0x60/0 x70)
[ 263.455915] r5:c04b3efc r4:ee65eb40
[ 263.466595] [<c036c74c>] (__vfs_getxattr) from [<c04dff60>] (get_vfs_caps_fro m_disk+0x6c/0x180)
[ 263.492609] r7:ed2d2200 r6:c1204c48 r5:ed2adea8 r4:cfdf6980
[ 263.509526] [<c04dfef4>] (get_vfs_caps_from_disk) from [<c04e0210>] (cap_bprm _set_creds+0x19c/0x540)
[ 263.536839] r8:c0c01c8c r7:ed2d2200 r6:00000001 r5:cfdf6200 r4:cfdf6980
[ 263.556878] [<c04e0074>] (cap_bprm_set_creds) from [<c034bd28>] (prepare_binp rm+0x138/0x18c)
[ 263.582113] r10:00000001 r9:00000000 r8:ed2a4e84 r7:00000000 r6:ee65eb40 r5: c1204c48
[ 263.605524] r4:ed2d2200
[ 263.613081] [<c034bbf0>] (prepare_binprm) from [<c034cfa0>] (__do_execve_file +0x478/0x738)
[ 263.637796] r8:ed2a4e84 r7:00000000 r6:ed2d2200 r5:ed452000 r4:c1204c48
[ 263.657833] [<c034cb28>] (__do_execve_file) from [<c034d2c8>] (do_execve+0x30 /0x38)
[ 263.680728] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5: ed2a4c40
[ 263.704139] r4:cfdf6200
[ 263.711697] [<c034d298>] (do_execve) from [<c0235134>] (call_usermodehelper_e xec_async+0x198/0x1c8)
[ 263.738755] [<c0234f9c>] (call_usermodehelper_exec_async) from [<c02010d8>] ( ret_from_fork+0x14/0x3c)
[ 263.766330] Exception stack(0xed2adfb0 to 0xed2adff8)
[ 263.781422] dfa0: 00000000 00000000 00000 000 00000000
[ 263.805877] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000 000 00000000
[ 263.830329] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
[ 263.850105] r7:00000000 r6:00000000 r5:c0234f9c r4:ed2a4c40
[ 263.871558] Invalid argument reading file caps for /lib/systemd/systemd-cored ump
[ 263.911028] Core dump to |/lib/systemd/systemd-coredump 308 0 0 7 1638956261 4294967295 k2g-evm sshd pipe failed