This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5535: Using Spectrum Digital ezDSP board (circa 2011) with CCS 11

Part Number: TMS320C5535


Hi - DSP noob, but eclipse veteran here. I'm hoping to do some basic DSP 101 type experiments on the SD ezDSP  eval board  (TMS320C5535) that's sat neglected in my desk for like 9 years. I've installed CCS 11(including the DSP and SD includes) , confirmed that the eval board actually works, plugged its USB J2 into the PC... my PC acknowledges the new USB device, but the CCS new project wizard does not find the connected board, and it doesn't seem to be in the board pulldown list.

I'm assuming that maybe CCS v11 doesn't recognize the connected board because I need to add a special config for this old board?

Any help or links appreciated. Happy holidays all.