Other Parts Discussed in Thread: TAS5634, DSD1796, DF1704
Hi,
My customer want find DSP can support DSD signal input, and can work with TAS5634 PWM input,
Do you have any suggestion?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer want find DSP can support DSD signal input, and can work with TAS5634 PWM input,
Do you have any suggestion?
Thanks!
Jeff
Jeff,
It seems to me " DSD1796 - 123dB SNR Stereo Audio DAC " supports both DSD and PCM formats.
https://www.ti.com/product/DSD1796
As per the datasheet of this DAC, this can be interfaced with DSP.
The following texts are the extracts from the datasheet.
The DSD1796 accepts the PCM and DSD audio data formats, providing easy interfacing to audio DSP and decoder chips. The DSD1796 also interfaces with external digital filter devices (DF1704, DF1706, PMD200). Sampling rates up to 200 kHz are supported. A full set of user-programmable functions is accessible through an SPI serial control port, which supports register write and readback functions
Regards
Shankari G