Part Number: TDA4VM
Other Parts Discussed in Thread: CDCE6214, CDCI6214
Hi TI:
We have some problem about CDCE6214 application in TDA4.
1.Is it must be have 50ohm to gnd between TDA4 and CDCE6214 100MHz clock? We can see it is must be have in ref design and datasheet based on CDCI6214.But it is not must have 50ohm to gnd at LP-HCSL mode in CDCE6214 datasheet.


2.The TDA4 require software close the internal termination before the ref clk is good,when the ref clk vpp is bigger than 400mV.(And that CDCE6214 ref clk vpp is always bigger than 400mV whether in LP-HCSL mode or LVDS mode.)So, the software need to close the internal termination and the TDA4 need to add external 50ohm to gnd in ref clk.Is that correct?Is it must be conterl the CDCE6214 not output ref clk in TDA4 power on?

3.Is the CDCE6214 work in LP-HCSL mode or LVDS mode with the TDA4?And is the ref clk need to have series AC capacitance when CDCE6214 work in LVDS mode ?
4.Is the function of series 30ohm and 50ohm to gnd between TDA4 and CDCI6214 100MHz clock in the tda4 ref design?
5.Do you have some design suggest about the TDA4 with CDCE6214?
Thanks!!