Part Number: TDA4VM
Hello,
I am having trouble capturing images from MIPI CSI2 image sensor using a Linux V4L2 driver.
Driver and device tree overlay implementations are based on the OV5640 implementation from the TI sources, SDK Linux J7 EVM 08_00_00_08.
The driver is probed and I2C communication works, but the frames do not arrive after the stream is enabled. There are no errors in kernel or application logs. However, I have confirmed that the sensor is sending data at configured frame rate using an oscilloscope.
The image sensor is connected directly to the CSI2RX0 port without SerDes.
Sensor configuration:
| Resolution | 3864x2192 |
| bpp | 10 |
| fps | 45 |
| lanes | 2 |
The v4l2-ctl tool is used to test the stream. The application is stuck after VIDIOC_STREAMON.
root@j7-evm:~# v4l2-ctl -d /dev/video1 -v 'width=3864,height=2192,pixelformat=9' --stream-mmap --verbose
VIDIOC_QUERYCAP: ok
VIDIOC_G_FMT: ok
VIDIOC_S_FMT: ok
Format Video Capture:
Width/Height : 3864/2192
Pixel Format : 'GB10' (10-bit Bayer GBGB/RGRG)
Field : None
Bytes per Line : 7728
Size Image : 8469888
Colorspace : sRGB
Transfer Function : Default (maps to sRGB)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Full Range)
Flags :
VIDIOC_REQBUFS returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_STREAMON returned 0 (Success)
Media controller topology seems to be set correctly.
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:4500000.ticsi2rx
hw revision 0x1
driver version 5.10.41
Device topology
- entity 1: cdns_csi2rx.4504000.csi-bridge (5 pads, 2 links)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
pad0: Sink
<- "imx415 10-001a":0 [ENABLED,IMMUTABLE]
pad1: Source
-> "j721e-csi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
pad3: Source
pad4: Source
- entity 7: imx415 10-001a (1 pad, 1 link)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev1
pad0: Source
[fmt:SGBRG10_1X10/3864x2192@1/45 field:none colorspace:srgb]
-> "cdns_csi2rx.4504000.csi-bridge":0 [ENABLED,IMMUTABLE]
- entity 11: j721e-csi2rx (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video1
pad0: Sink
<- "cdns_csi2rx.4504000.csi-bridge":1 [ENABLED,IMMUTABLE]
Below are the values of CSI2RX0 related registers when the v4l2-ctl is stuck waiting for frames.
R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_DEVICE_CONFIG 0x00000013 0x8C63164C R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_SOFT_RESET 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STATIC_CFG 0x00000013 0x43210200 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ERROR_BYPASS_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_MONITOR_IRQS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_MONITOR_IRQS_MASK_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_INFO_IRQS 0x00000013 0x00000030 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_INFO_IRQS_MASK_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ERROR_IRQS 0x00000013 0x00000120 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ERROR_IRQS_MASK_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_DPHY_LANE_CONTROL 0x00000013 0x00013013 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_DPHY_STATUS 0x00000013 0x00222206 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_DPHY_ERR_STATUS_IRQ 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_DPHY_ERR_IRQ_MASK_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_INTEGRATION_DEBUG 0x00000013 0x10000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ERROR_DEBUG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_TEST_GENERIC 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_CTRL 0x00000013 0x00000001 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_STATUS 0x00000013 0x80000111 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_DATA_CFG 0x00000013 0x00010000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_CFG 0x00000013 0x00000100 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_MONITOR_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_MONITOR_FRAME 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_MONITOR_LB 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_TIMER 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_FCC_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_FCC_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM0_FIFO_FILL_LVL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_STATUS 0x00000013 0x80000111 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_DATA_CFG 0x00000013 0x00010000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_CFG 0x00000013 0x00000100 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_MONITOR_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_MONITOR_FRAME 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_MONITOR_LB 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_TIMER 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_FCC_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_FCC_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM1_FIFO_FILL_LVL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_CTRL 0x00000013 0x00000001 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_STATUS 0x00000013 0x80000111 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_DATA_CFG 0x00000013 0x00010000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_CFG 0x00000013 0x00000100 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_MONITOR_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_MONITOR_FRAME 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_MONITOR_LB 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_TIMER 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_FCC_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_FCC_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM2_FIFO_FILL_LVL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_CTRL 0x00000013 0x00000001 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_STATUS 0x00000013 0x80000111 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_DATA_CFG 0x00000013 0x00010000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_CFG 0x00000013 0x00000100 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_MONITOR_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_MONITOR_FRAME 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_MONITOR_LB 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_TIMER 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_FCC_CFG 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_FCC_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_STREAM3_FIFO_FILL_LVL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_INT_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_INT_RAW_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_INT_MASK 0x00000013 0x0000007F R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_INT_TEST 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_FATAL_NONFATAL_SELECT 0x00000013 0x0000007F R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_SRAM_CORR_FAULT_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_SRAM_UNCORR_FAULT_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_SRAM_FAULT_STATS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_TRANS_TO_CTRL 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_TRANS_TO_FAULT_MASK 0x00000013 0x00000001 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_TRANS_TO_FAULT_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_PROTOCOL_FAULT_MASK 0x00000013 0x00003FFF R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ASF_PROTOCOL_FAULT_STATUS 0x00000013 0x00000000 R CSI_RX_IF_VBUS2APB0_CSI_RX_IF_VBUS2APB_ID_PROD_VER 0x00000013 0x50220200 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_REV 0x00000013 0x66A0EA00 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_VECTOR 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_STAT 0x00000013 0x00000008 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_RESERVED_SVBUS_y 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_SEC_EOI_REG 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_SEC_STATUS_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_SEC_ENABLE_SET_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_SEC_ENABLE_CLR_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_DED_EOI_REG 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_DED_STATUS_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_DED_ENABLE_SET_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_DED_ENABLE_CLR_REG0 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_AGGR_ENABLE_SET 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_AGGR_ENABLE_CLR 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_AGGR_STATUS_SET 0x00000013 0x00000000 R CSI_RX_IF0_ECC_AGGR_CFG_CSI_RX_IF_ECC_AGGR_STATUS_CLR 0x00000013 0x00000000 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_CSIRX_ID 0x00000013 0x64706100 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_VP0 0x00000013 0x00000000 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_VP1 0x00000013 0x00000000 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_CNTL 0x00000013 0x00000F01 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_DMACNTX 0x00000013 0x8000002B R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_PSI_CFG0 0x00000013 0x00008000 R CSI_RX_IF0_RX_SHIM_VBUSP_MMR_CSI2RXIF_CSI_RX_IF_SHIM_PSI_CFG1 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_REVISION 0x00000013 0x6690A200 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_EOI_REG 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_INTR_VECTOR_REG 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_ENABLE_REG_LEVEL_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_ENABLE_REG_PULSE_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_ENABLE_CLR_REG_LEVEL_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_ENABLE_CLR_REG_PULSE_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_STATUS_REG_LEVEL_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_STATUS_REG_PULSE_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_STATUS_CLR_REG_LEVEL_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_STATUS_CLR_REG_PULSE_0 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_INTR_VECTOR_REG_LEVEL 0x00000013 0x00000000 R CSI_RX_IF0_CP_INTD_CFG_INTD_CFG_CSI_RX_IF_CP_INTD_INTR_VECTOR_REG_PULSE 0x00000013 0x00000000 R DPHY_RX0_MMR_SLV_K3_DPHY_WRAP_DPHY_RX_MMR_SLV_LANE 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_ANA_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT0 0x00000013 0x00001140 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT2 0x00000013 0x00000429 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT3 0x00000013 0x05030101 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT4 0x00000013 0x0032011E R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT5 0x00000013 0x00000400 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT6 0x00000013 0x000400C8 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT7 0x00000013 0x000300C8 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT8 0x00000013 0x00080103 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT10 0x00000013 0x00800000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT11 0x00000013 0x00000015 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT12 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT13 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT14 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT20 0x00000013 0x00000140 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT21 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT22 0x00000013 0x00000694 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT23 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT24 0x00000013 0x0F0501B0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT25 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT26 0x00000013 0x0000000A R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT27 0x00000013 0xDECDBCAB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT28 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT31 0x00000013 0x00040400 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT32 0x00000013 0x00000201 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT33 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT34 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT35 0x00000013 0x001380BB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT36 0x00000013 0x00000EE8 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT37 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT38 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT39 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT50 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT53 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT54 0x00000013 0x00000002 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT56 0x00000013 0x0EE2E803 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CMN0_CMN_DIG_TBIT58 0x00000013 0x00000023 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_ANA_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_CLK0_RX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT10 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT11 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT12 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT13 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT14 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT15 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT16 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT17 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT18 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT19 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT20 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT21 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT22 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT23 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT24 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT25 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT26 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT27 0x00000013 0x0A000018 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT28 0x00000013 0xDECDBCAB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT29 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT30 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT31 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT32 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT33 0x00000013 0x010DD0DC R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT34 0x00000013 0x00008000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT35 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT36 0x00000013 0x0024A483 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT37 0x00000013 0x3E3EFBE7 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT38 0x00000013 0x0010200D R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT39 0x00000013 0x01001015 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT40 0x00000013 0x00101405 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT41 0x00000013 0x00040011 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT42 0x00000013 0x0041880D R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT43 0x00000013 0x0052CA5B R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT44 0x00000013 0x000058A0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT45 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT46 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT47 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT48 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT49 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT50 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL0_RX_DIG_TBIT51 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT10 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT11 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT12 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT13 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT14 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT15 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT16 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT17 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT18 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT19 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT20 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT21 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT22 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT23 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT24 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT25 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT26 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT27 0x00000013 0x0A000018 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT28 0x00000013 0xDECDBCAB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT29 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT30 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT31 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT32 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT33 0x00000013 0x010DD05C R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT34 0x00000013 0x00008000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT35 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT36 0x00000013 0x0062E083 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT37 0x00000013 0x3E3EFC07 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT38 0x00000013 0x00105C2D R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT39 0x00000013 0x00160031 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT40 0x00000013 0x00105425 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT41 0x00000013 0x0114002D R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT42 0x00000013 0x00400800 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT43 0x00000013 0x00010020 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT44 0x00000013 0x000058A0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT45 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT46 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT47 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT48 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT49 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT50 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL1_RX_DIG_TBIT51 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT10 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT11 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT12 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT13 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT14 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT15 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT16 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT17 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT18 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT19 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT20 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT21 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT22 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT23 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT24 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT25 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT26 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT27 0x00000013 0x0A000018 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT28 0x00000013 0xDECDBCAB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT29 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT30 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT31 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT32 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT33 0x00000013 0x00008000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT34 0x00000013 0x00044000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT35 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT36 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT37 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT38 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT39 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT40 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT41 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT42 0x00000013 0x00400800 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT43 0x00000013 0x00010020 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT44 0x00000013 0x000058A0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT45 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT46 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT47 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT48 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT49 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT50 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL2_RX_DIG_TBIT51 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_ANA_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_ANA_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT4 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT5 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT10 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT11 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT12 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT13 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT14 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT15 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT16 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT17 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT18 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT19 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT20 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT21 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT22 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT23 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT24 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT25 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT26 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT27 0x00000013 0x0A000018 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT28 0x00000013 0xDECDBCAB R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT29 0x00000013 0x00000028 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT30 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT31 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT32 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_ANA_TBIT2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT33 0x00000013 0x00008000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT34 0x00000013 0x00044000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT35 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT36 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT37 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT38 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT39 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT40 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT41 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT42 0x00000013 0x00400800 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT43 0x00000013 0x00010020 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT44 0x00000013 0x000058A0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT45 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT46 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT47 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT48 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT49 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT50 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_DL3_RX_DIG_TBIT51 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT0 0x00000013 0x000002B5 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT2 0x00000013 0xAAAAAAAA R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT3 0x00000013 0x000000AA R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT4 0x00000013 0x22222222 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT5 0x00000013 0x00000222 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT6 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT7 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT8 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT9 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_PCS_TX_DIG_TBIT10 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_CNTRL 0x00000013 0x0000050F R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_RESET 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_ENABLE 0x00000013 0x0000010F R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_CMN_CTRL 0x00000013 0x000000E0 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_CL_CNTRL_L 0x00000013 0x0000002D R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_CTRL_L0 0x00000013 0x00000005 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_HS_L0 0x00000013 0x00000530 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_RX_ESC_L0 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_CTRL_L1 0x00000013 0x00000005 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_HS_L1 0x00000013 0x000005D1 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_DL_RX_ESC_L1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_PHY_ISO_SPARE_1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_CTRL_L2 0x00000013 0x00000004 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_HS_L2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_RX_ESC_L2 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_CTRL_L3 0x00000013 0x00000004 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_HS_L3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_DL_RX_ESC_L3 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_RX_SPARE_1 0x00000013 0x00000000 R DPHY_RX0_VBUS2APB_WRAP_VBUSP_K3_DPHY_RX_DPHY_RX_VBUS2APB_ISO_LDD_PHY_ISO_RX_SPARE_2 0x00000013 0x00000000
As a side note, the sensor works with an RTOS driver implemented as described in the RTOS Developer Note.
Any suggestions on how to proceed with debugging are appreciated.