This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4 sd boot failed

Part Number: TDA4VM

Hi TI:

We find 1pcs PCBA boot failed in SD boot mode at ourself TDA4 board .

Could you tell me some suggest?

There are some information as follow:

Processors: TDA4

Boot mode :SD 

SDK :8.0

Log:

U-Boot SPL 2021.01 (Oct 11 2021 - 17:29:10 +0800)
Model: Texas Instruments K3 J721E SoC
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
Board: J721EX-PM1-SOM rev E2
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed 1
Trying to boot from MMC2
spl_load_image_fat: error reading image tispl.bin, err - -6
spl_load_image_ext: ext4fs mount err - 0
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

Thanks!!