Hello,
I found the pcie interface can't work normally now, which can't detect the device(e1000e nic which works well in other board).
Run lspci can't get anything and I got below logs. Any hints? thanks a lot!
PS: I tried TI816XPSP_04.00.00.07 and TI816XPSP_04.00.00.08, both have same problem.
ti816x_pcie: Invoking PCI BIOS...
ti816x_pcie: Setting up Host Controller...
ti816x_pcie: Register base mapped @0xf0808000
ti816x_pcie: Setting outbound translation for 0x20000000-0x2fffffff
ti816x_pcie: Starting PCI scan...
pci_bus 0000:00: scanning bus
ti816x_pcie: Reading config[0] for device 0000:00:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:01:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:02:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:03:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:04:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:05:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:06:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:07:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:08:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:09:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0a:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0b:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0c:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0d:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0e:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:0f:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:10:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:11:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:12:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:13:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:14:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:15:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:16:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:17:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:18:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:19:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1a:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1b:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1c:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1d:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1e:00..
failed. No link/device.
ti816x_pcie: Reading config[0] for device 0000:1f:00..
failed. No link/device.
pci_bus 0000:00: fixups for bus
PCI: bus0: Fast back to back transfers enabled
pci_bus 0000:00: bus scan returning with max=00
pci_bus 0000:00: resource 0 [mem 0x20000000-0x2fffffff]
pci_bus 0000:00: resource 1 [io 0x40000000-0x402fffff]
Best regards
Gary