Part Number: AM3357
Hi,
I have few queries for AM3357 device.
- What is the use case of CPSW interface which uses RMII interface ? Does it support HSR / PTP or it is just a MAC based Ethernet interface ?
- In order to use HSR with PTPV2 what is the configuration to be used ? Is it PRU-ICSS MII interface ? Can we use RMII interface with PRU-ICSS ?
- In order to use HSR with PTPV1 what is the configuration to be used ? Is it PRU-ICSS MII interface ? Can we use RMII interface with PRU-ICSS ?
- How to configure between PTPV1 and PTPV2 ?
- Please find attached file for pin muxing for the Ethernet MII with PRU-ICSS which shows conflict between T17 pin for using it for NAND flash interfacing in 8 bit boot mode & PRU-ICSS. How to resolve this conflict ? Changing NAND flash to eMMC just for this pin conflict is not a good idea due to cost impact between two memories.
- From below link the jumper setting for ICE board is for CPSW & PRU-ICSS configuration & not for MII + PTPV1 or MII + PTPV2 configuration. If yes how to configure the PTPV1 and PTPV2 ? Please clarify https://software-dl.ti.com/processor-sdk-linux/esd/docs/05_02_00_10/linux/Foundational_Components_PRU-ICSS_PRU_ICSSG.html#pru-icss-ethernet
Regards,
Dushyant