Dear TI,
I need a specific design between CS and SPI clock for delay above 20us. But it seems to be too short for the default McSPI setting.
Here're some method that I want to use
1. Can I add delay time in spi-omap2-mcspi.c ? If yes, where can I add it ?
2. Use additional GPIO pin as CS pin to control ?
or Is there any method to solve ?
Thanks a lot.
BR.