Other Parts Discussed in Thread: OMAP-L138
Hi,
We have two LogicPD OMAP-L138 Kits.
When we check the ROM revision for the kits @ Address 0xFFFD 0000, on one of the kit the ROM version is read as d800k004 and on another kit it is read as d800k006.
Is it important to select this version from the AISgen application while generating the AIS file?
Because once we go for production first we have to check which ROM Version of the processor I am using and then I have to program the corresponding AIS file which is a little time consuming if I am programming say 50 or 100 Devices.
Please clarify how important is this? So for example if we program a AIS File to the NAND which is generated by selecting the device type as d800k006?
Regards,
GSR