This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6437 video port: using data output formatter



I want to use the dm6437 video output formatter when processing a raw image.  The documentation for setting up the registers is a little fuzzy to me.  If I want x lines written to SRAM after the video data formatter, what values do I need to use for these registers?  I can adjust the number of lines output by the camera to whatever I want.  Also, since the output has to be at least 1 line less than the input, which line(s) are eaten by the output formatter?  First or last?

FMT_VERT

VP_OUT

VERT_LINES

VERT_START

I figured I would set up the camera to output x + 2 lines (since it is raw bayer the length has to be even).  What are my other register values (relating to the height)?