This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TMS320C6657: How to create "Target configuration" and do "Test connection" on C6657 EVM

Part Number: TMS320C6657

Hi,

How to create "Target configuration" and do "Test connection" on C6657 EVM ?

  • Pre-requisite 

    1. Install CCS 9.3 from CCSTUDIO_9.3.0.00012 | TI.com
    2. In your C6657 EVM - board ----> You should put the DIP Switch settings in "No boot mode"  to connect to the CCS.

      That is  ------> DIP SW3 : 0 1 1 1 1 1 1 1 and DIP SW5 : 1 1 1 1 1 1 1 1

    Connection Details:

    -----

    Either download this video before watching or use the maximize button, " [[ ]]"  before playing.

    Please follow the steps as per the video, below.

    Output screenshot:

    Regards

    Shankari G