I have seen similar problem asked many times, but I still don't understand it very well.I have to admit the PRTCSS module is very confusing to me.
Our DM368 is powered by TPS65023, it has a super cap onboard as backup supply. We are trying to use normal mode: the PWRST and PWRCNTON are both connected to 1.35V, which I confirmed stays on when main power is removed. Now after the power up, the RTC goes back to zero every time. My understanding is that if both PWRST and PWRCNTON are high, the RTC module should not be reset.
Please help me if you have experience with such problem, thanks!