Hello,
I'm getting an unexpected error when making a call to System_printf in a SWI. The SWI runs fine without it, but if adding that in (as needed), it reports the following error after generating the console text specified in the System_printf:
ti.sysbios.gates.GateMutex: line 114: assertion failure: A_badContext: bad calling context. See GateMutex API doc for details.
xdc.runtime.Error.raise: terminating execution
Any help with debugging this would be appreciated.
Robert
IPC 1.22.3.23
SYS/BIOS 6.31.4.27
XDAIS 6.23
XDC 3.20.7.86