Part Number: AM3358
I'm attempting to simulate my layout for the AM3358-ZCZ MII peripheral. Pin U14 needs to be in Mode 1 to be GMII_TXD3 as an example of what I need to configure. I'm using the sprm552c.ibs model and can see that pin U14 points to Selector_15. Sel_15 has 18 configurations to choose from... My IO is running 3.3V so that narrows the choices, and I assume 100Mb has the pull-up and pull-down resistors disabled, and is running with a fast slew-rate. That drops me to Model_199 (5% PS) or Model_211 (10% PS). Is that correct logic to select the driver for Mode 1 MII?