Part Number: TDA4VM
Greetings TI,
Merry Christmas and a Happy New Year.
How to change TDA4 C66x PLL core clocks in Linux from the shell?
Used Linux SDK: 08.00.01.10.
Thanks,
Alexey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Greetings TI,
Merry Christmas and a Happy New Year.
How to change TDA4 C66x PLL core clocks in Linux from the shell?
Used Linux SDK: 08.00.01.10.
Thanks,
Alexey
Hi Alexey,
You can use k3conf to change the clock frequency.
The following application note has an example for C7x, and it can be adapted for C6x as well.
Refer to Page 17 (Strategy 5)
Regards
Karthik
Karthik,
The thing is that using k3conf I can change every clock of TDA4VM exepct C66x domain.
Regards,
Alexey
Alexey,
Ah, ok.. this is strange.
Could you please share more details about what you have tried and how you verified that the C6x clock is not changing?
It would useful to clarify the SDK version that you are using as well. We will replicate the issue and enable you further.
Regards
Karthik
Karthik,
This is what I get:
root@j7-evm:/run/media/sdb# k3conf dump device 143
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Thu Sep 2 18:06:41 UTC 2021) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0015 '21.5.0--v2021.05 (Terrific Llam)') |
|--------------------------------------------------------------------------------|
|------------------------------------------------------|
| Device ID | Device Name | Device Status |
|------------------------------------------------------|
| 143 | J721E_DEV_C66SS1_CORE0 | DEVICE_STATE_ON |
|------------------------------------------------------|
root@j7-evm:/run/media/sdb# k3conf dump clock 143
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Thu Sep 2 18:06:41 UTC 2021) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0015 '21.5.0--v2021.05 (Terrific Llam)') |
|--------------------------------------------------------------------------------|
|-----------------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-----------------------------------------------------------------------------------------------|
| 143 | 0 | DEV_C66SS1_CORE0_GEM_TRC_CLK | CLK_STATE_READY | 0 |
| 143 | 1 | DEV_C66SS1_CORE0_GEM_CLK2_OUT_CLK | CLK_STATE_READY | 0 |
| 143 | 4 | DEV_C66SS1_CORE0_GEM_PBIST_ROM_CLK | CLK_STATE_READY | 0 |
| 143 | 6 | DEV_C66SS1_CORE0_GEM_CLKIN_CLK | CLK_STATE_READY | 1350000000 |
|-----------------------------------------------------------------------------------------------|
root@j7-evm:/run/media/sdb# k3conf set clock 143 6 1000000000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Thu Sep 2 18:06:41 UTC 2021) |
| SoC | J721E SR2.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0015 '21.5.0--v2021.05 (Terrific Llam)') |
|--------------------------------------------------------------------------------|
Invalid clock arguments
COMMANDS
k3conf set clock <dev_id> <clk_id> <freq>
Sets the clock frequency and prints the status
Regards,
Alexey
Hi Alexey,
I could reproduce the issue with k3confi that you have highlighted above.
I tried playing around a bit more and it works only with 1350000000 which is the default set frequency.
k3conf set clock 143 6 1350000000
|--------------------------------------------------------------------------------|
| VERSION INFO |
|--------------------------------------------------------------------------------|
| K3CONF | (version v0.1-45-g79f007c built Mon Dec 20 16:35:52 UTC 2021) |
| SoC | J721E SR1.0 |
| SYSFW | ABI: 3.1 (firmware version 0x0015 '21.9.1--v2021.09a (Terrific Lla)') |
|--------------------------------------------------------------------------------|
|-----------------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-----------------------------------------------------------------------------------------------|
| 143 | 0 | DEV_C66SS1_CORE0_GEM_TRC_CLK | CLK_STATE_READY | 0 |
| 143 | 1 | DEV_C66SS1_CORE0_GEM_CLK2_OUT_CLK | CLK_STATE_READY | 0 |
| 143 | 4 | DEV_C66SS1_CORE0_GEM_PBIST_ROM_CLK | CLK_STATE_READY | 0 |
| 143 | 6 | DEV_C66SS1_CORE0_GEM_CLKIN_CLK | CLK_STATE_READY | 1350000000 |
|-----------------------------------------------------------------------------------------------|
What is your final intent. I need to check with our HW experts on what other frequencies C6x can run normally.
Can you describe your use case and what you are trying to achieve by reducing the C6x clock frequency?
- Keerthy
Keerthy,
My final usecase to extend working time by lowering freqency and power consumption of high current domains due to normally staying in stand-by (less than 3% of perfomance used) mode. The final goal to extend power consumption to one day of internal power reserve (3-4W/h).
Regards,
Alexey
Alexey,
Thanks for the detailed use case. I will check internally and get back if we can reduce the C6x clock frequency dynamically.
Best Regards,
Keerthy
Hi Alexey,
Can you try directly writing the registers:
devmem2 0x68D030 w 0x68 devmem2 0x68D034 w 0x00800000
PLL13_FREQ_CTRL0 & PLL13_FREQ_CTRL1 registers to cater to C6x frequency changes.
root@j7-evm:~# k3conf dump clock 143
|-----------------------------------------------------------------------------------------------|
| Device ID | Clock ID | Clock Name | Status | Clock Frequency |
|-----------------------------------------------------------------------------------------------|
| 143 | 0 | DEV_C66SS1_CORE0_GEM_TRC_CLK | CLK_STATE_READY | 0 |
| 143 | 1 | DEV_C66SS1_CORE0_GEM_CLK2_OUT_CLK | CLK_STATE_READY | 0 |
| 143 | 4 | DEV_C66SS1_CORE0_GEM_PBIST_ROM_CLK | CLK_STATE_READY | 0 |
| 143 | 6 | DEV_C66SS1_CORE0_GEM_CLKIN_CLK | CLK_STATE_READY | 1003200000 |
|-----------------------------------------------------------------------------------------------|
Best Regards,
Keerthy