This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: QMSS

Part Number: TMS320C6678


Hi,

After the customer initializes the QMSS using the interface setupQmCdma() provided by TI, when calling Qmss_queuePop(), the descriptor is empty, Please help analyze.

  • Nancy,

    The sequence of initialization and configuration of (QMSS initialization, QMSS open, QMSS queue pop ) are demonstrated in the PDK example, cppi_evmc6678_C66BiosTestProject  located at  " \pdk_c667x_2_0_16\packages\MyExampleProjects\cppi_evmc6678_C66BiosTestProject" .

    I have just tested this example on C6678 EVM, today and it seems to be successfully working.

    So, it is a better choice to request the customer to compare the sequence of qmss portion w.r.t this example code.

    If they have one C6678 EVM, please do ask them to run, compare and analyze with their setup.

    Regards

    Shankari G

  • Nancy,

    I haven't heard back. Assuming it is resolved.

    Regards

    Shankari G