This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM572X: dynamic loader error

Part Number: TMDSEVM572X

Hi,

When we tried to compile our application in the AM5728-evm we got the following error:

CMake Error at CMakeLists.txt:191 (message):
  Could not find the standard dynamic loader at /lib/ld-linux.so.2

So we modified the makefile accordingly to consider the processor-sdk-linux  loader : ld-linux-armhf.so.3

But now after the modification we are getting the following error:

c++: error: unrecognized command line option '-msse2'                           
c++: error: unrecognized command line option '-mfpmath=sse'                     

make[2]: *** [libraries/wireless/CMakeFiles/shptoxml.dir/build.make:63: librarie
s/wireless/CMakeFiles/shptoxml.dir/src/shptoxml/shptoxml.cpp.o] Error 1         
make[1]: *** [CMakeFiles/Makefile2:624: libraries/wireless/CMakeFiles/shptoxml.d
ir/all] Error 2                                                                 
make: *** [Makefile:139: all] Error 2

SDK used in the platform: PROCESSOR-SDK-LINUX-RT-AM57X

Request you suggest the suitable solution at the earliest.Thanks in advance