Part Number: TDA4VM
when i test IPC between mcu_1_0 and A72,
i kill the user process which read "ti_rpmsg_char" by "read" function,
then A72 output "virtio_rpmsg_bus virtio3: msg received with no recipient"
Question_1:
is ti_rpmsg_char(which running in linux kernel space) consume the IPC data? and drop it ? if no "user space process"(which read the data by "read")
because i can not detect mailbox full by "HW_RD_REG32(tx_baseAddr + MAILBOX_FIFOSTATUS(tx_queueId))" in mcu_1_0
Question_2:
i checked datasheet about "MAILBOX_MSG_STATUS_y Register" and found "NUM_MESSAGES(bit2,10)",so the max NUM_MESSAGES value is 7
is mailbox max FIFO depth == 7?