This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: The MCAN drive SD is not functional

Part Number: TDA4VM

Hi team,

Here's an issue from the customer may need your help:

The CAN drive is tuned in the path pdk_jacinto_08_00_00_37\packages\ti\csl\example\mcan and the test data is simulated on the EVM board.

The customer wants to try the SD card startup, but there is no free rtos system in this example, and the SD card must have a free rtos system, or something like that. So it's organized into ca_driver.c called in another example, such as ipc(ti-processor-sdk-rtos-j721e-evm-08_00_00_12\pdk_jacinto_08_00_00_37\packages\ti\drv\ipc) Or eth(ti-processor-sdk-rtos-j721e-evm-08_00_00_12\ti-processor-sdk-rtos-j721e-evm-08_00_12\ethfw\ Examples of apps\app_remoteswitchcfg_server).

The integrated CCS simulation test has CAN data. But the SD card is stuck in the CAN initialization. The environment is the EVM board. The customer would like to know why is that?

Could you help check this case? Thanks.

Best Regards,

Cherry