Part Number: AM6442
Other Parts Discussed in Thread: DP83869
Hi,
I have a custom PCB with AM6442 SoC and a DP83869 PHY connected to CPSW.
The interface is 1000M RGMII, copper.
I'm using Linux SDK 08.00.00.004.
I'm trying to bring up the ehternet interface in U-boot.
I could not find a driver for this PHY in the SDK, so I'm using the following patch:
https://patches.linaro.org/project/u-boot/patch/20200420185310.6630-3-dmurphy@ti.com/
I had to fix this patch in order to work in U-boot, for example:
* Usage of CONFIG_OF_MDIO, which is never defined in U-boot, this is a Linux macro. (replaced it with CONFIG_DM_ETH).
* Usage of of_property_read_u32 and of_property_read_bool, which are Linux kernel functions, not U-boot's (replaced with the U-boot equivalent ofnode_read_u32 and ofnode_read_bool)
* Some differences in struct dp83869_private and ofnode of_node.
After All these changes, U-boot compiles without any error or warnings.
But, when I use this U-boot, I get am65_cpsw_nuss_slave errors:
Net: phy_device_create, PHY probe failed phy_device_create, PHY probe failed phy_device_create, PHY probe failed phy_device_create, PHY probe failed phy_device_create, PHY probe failed phy_device_create, PHY probe failed Could not get PHY for ethernet@8000000: addr 0 am65_cpsw_nuss_slave ethernet@8000000: phy_connect() failed No ethernet found.
I tried to debug this, without success.
I tried to use generic PHY driver and implement a board_phy_config function in my board directory.
I wrote to the MDIO register following DP83869's datasheet instructions(RGMII to COPPER) without sucess
https://www.ti.com/lit/ds/symlink/dp83869hm.pdf#page=38
Datasheet instructions:
9.4.8.1 RGMII-to-Copper Ethernet Mode After configuring register 0x01DF, perform the following operations. • Write 0x1140 to register 0x0000 • Write 0x5048 to register 0x0010 • Write 0x0B00 to register 0x0009
Attaching registers dump:
=> mii read 0 0 1140 => mii read 0 0x10 5048 => mii read 0 0x9 0B00 => mii dump 0 0 0. (1140) -- PHY control register -- (8000:0000) 0.15 = 0 reset (4000:0000) 0.14 = 0 loopback (2040:0040) 0. 6,13 = b10 speed selection = 1000 Mbps (1000:1000) 0.12 = 1 A/N enable (0800:0000) 0.11 = 0 power-down (0400:0000) 0.10 = 0 isolate (0200:0000) 0. 9 = 0 restart A/N (0100:0100) 0. 8 = 1 duplex = full (0080:0000) 0. 7 = 0 collision test enable (003f:0000) 0. 5- 0 = 0 (reserved) => mii dump 0 1 1. (796d) -- PHY status register -- (8000:0000) 1.15 = 0 100BASE-T4 able (4000:4000) 1.14 = 1 100BASE-X full duplex able (2000:2000) 1.13 = 1 100BASE-X half duplex able (1000:1000) 1.12 = 1 10 Mbps full duplex able (0800:0800) 1.11 = 1 10 Mbps half duplex able (0400:0000) 1.10 = 0 100BASE-T2 full duplex able (0200:0000) 1. 9 = 0 100BASE-T2 half duplex able (0100:0100) 1. 8 = 1 extended status (0080:0000) 1. 7 = 0 (reserved) (0040:0040) 1. 6 = 1 MF preamble suppression (0020:0020) 1. 5 = 1 A/N complete (0010:0000) 1. 4 = 0 remote fault (0008:0008) 1. 3 = 1 A/N able (0004:0004) 1. 2 = 1 link status (0002:0000) 1. 1 = 0 jabber detect (0001:0001) 1. 0 = 1 extended capabilities
Then, I try to use dhcp command without success:
=> dhcp ethernet@8000000 Waiting for PHY auto negotiation to complete.. done link up on port 1, speed 1000, full duplex BOOTP broadcast 1 BOOTP broadcast 2 BOOTP broadcast 3 BOOTP broadcast 4 BOOTP broadcast 5 BOOTP broadcast 6 BOOTP broadcast 7 BOOTP broadcast 8 BOOTP broadcast 9 BOOTP broadcast 10 BOOTP broadcast 11
I suspect that MAC is not sending the packets, I sniffed the network from a different machine in the same LAN, and got nothing..
The ethernet interface works in Linux, so this is a SW issue
# udhcpc udhcpc: started, v1.31.1 [ 11.960157] TI DP83869 8000f00.mdio:00: attached PHY driver [TI DP83869] (mii_bus:phy_addr=8000f00.mdio:00, irq=POLL) [ 11.973963] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down udhcpc: sending discover udhcpc: sending discover [ 16.066844] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off udhcpc: sending discover udhcpc: sending select for 192.168.15.118 udhcpc: lease of 192.168.15.118 obtained, lease time 86400 deleting routers adding dns 192.168.15.1 # ping 8.8.8.8 PING 8.8.8.8 (8.8.8.8) 56(84) bytes of data. 64 bytes from 8.8.8.8: icmp_seq=1 ttl=115 time=53.0 ms 64 bytes from 8.8.8.8: icmp_seq=2 ttl=115 time=52.7 ms 64 bytes from 8.8.8.8: icmp_seq=3 ttl=115 time=52.1 ms
How can I fix this?
Thanks.