Part Number: AM3358
Hi,
I'm using AM3358BZCZ80 to connect to icplus 1001c (phy chip)
use environment
- CPU : AM3358BZCZ80
- Linux Version : 4.1.18
* am335x dtsi
mac: ethernet@4a100000 {
compatible = "ti,am335x-cpsw","ti,cpsw";
ti,hwmods = "cpgmac0";
clocks = <&cpsw_125mhz_gclk>, <&cpsw_cpts_rft_clk>;
clock-names = "fck", "cpts";
cpdma_channels = <8>;
ale_entries = <1024>;
bd_ram_size = <0x2000>;
no_bd_ram = <0>;
rx_descs = <64>;
mac_control = <0x20>;
slaves = <2>;
active_slave = <0>;
cpts_clock_mult = <0x80000000>;
cpts_clock_shift = <29>;
reg = <0x4a100000 0x800
0x4a101200 0x100>;
#address-cells = <1>;
#size-cells = <1>;
interrupt-parent = <&intc>;
/*
* c0_rx_thresh_pend
* c0_rx_pend
* c0_tx_pend
* c0_misc_pend
*/
interrupts = <40 41 42 43>;
ranges;
syscon = <&scm_conf>;
status = "disabled";
davinci_mdio: mdio@4a101000 {
compatible = "ti,davinci_mdio";
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "davinci_mdio";
bus_freq = <1000000>;
reg = <0x4a101000 0x100>;
status = "disabled";
};
cpsw_emac0: slave@4a100200 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
cpsw_emac1: slave@4a100300 {
/* Filled in by U-Boot */
mac-address = [ 00 00 00 00 00 00 ];
};
phy_sel: cpsw-phy-sel@44e10650 {
compatible = "ti,am3352-cpsw-phy-sel";
reg= <0x44e10650 0x4>;
reg-names = "gmii-sel";
};
};
am335x.dts
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1 */
0x114 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txen.rgmii1_tctl */
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxdv.rgmii1_rctl */
0x11c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd3.rgmii1_td3 */
0x120 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd2.rgmii1_td2 */
0x124 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd1.rgmii1_td1 */
0x128 (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txd0.rgmii1_td0 */
0x12c (PIN_OUTPUT_PULLDOWN | MUX_MODE2) /* mii1_txclk.rgmii1_tclk */
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxclk.rgmii1_rclk */
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd3.rgmii1_rd3 */
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd2.rgmii1_rd2 */
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd1.rgmii1_rd1 */
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE2) /* mii1_rxd0.rgmii1_rd0 */
>;
};
cpsw_sleep: cpsw_sleep {
pinctrl-single,pins = <
/* Slave 1 reset value */
0x114 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x118 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x11c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x120 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x124 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x128 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x12c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x130 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x134 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x138 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x13c (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x140 (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
davinci_mdio_default: davinci_f_default {
pinctrl-single,pins = <
/* MDIO */
0x148 (PIN_INPUT_PULLUP | SLEWCTRL_FAST | MUX_MODE0) /* mdio_data.mdio_data */
0x14c (PIN_OUTPUT_PULLUP | MUX_MODE0) /* mdio_clk.mdio_clk */
>;
};
davinci_mdio_sleep: davinci_mdio_sleep {
pinctrl-single,pins = <
/* MDIO reset value */
0x148 (PIN_INPUT_PULLDOWN | MUX_MODE7)
0x14c (PIN_INPUT_PULLDOWN | MUX_MODE7)
>;
};
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rgmii-txid";
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "rgmii-txid";
};
Debug info as below :
In the current firmware, the PHY address is set to 3, and Ethernet related information is checked and linking is confirmed as shown below.

root@am335x-evm:~# ethtool -S eth0
NIC statistics:
Good Rx Frames: 1214
Broadcast Rx Frames: 454
Multicast Rx Frames: 713
Pause Rx Frames: 0
Rx CRC Errors: 0
Rx Align/Code Errors: 0
Oversize Rx Frames: 0
Rx Jabbers: 0
Undersize (Short) Rx Frames: 0
Rx Fragments: 0
Rx Octets: 159129
Good Tx Frames: 5
Broadcast Tx Frames: 5
Multicast Tx Frames: 0
Pause Tx Frames: 0
Deferred Tx Frames: 0
Collisions: 0
Single Collision Tx Frames: 0
Multiple Collision Tx Frames: 0
Excessive Collisions: 0
Late Collisions: 0
Tx Underrun: 0
Carrier Sense Errors: 0
Tx Octets: 359
Rx + Tx 64 Octet Frames: 244
Rx + Tx 65-127 Octet Frames: 669
Rx + Tx 128-255 Octet Frames: 165
Rx + Tx 256-511 Octet Frames: 127
Rx + Tx 512-1023 Octet Frames: 14
Rx + Tx 1024-Up Octet Frames: 0
Net Octets: 159488
Rx Start of Frame Overruns: 0
Rx Middle of Frame Overruns: 0
Rx DMA Overruns: 0
Rx DMA chan: head_enqueue: 1
Rx DMA chan: tail_enqueue: 517
Rx DMA chan: pad_enqueue: 0
Rx DMA chan: misqueued: 0
Rx DMA chan: desc_alloc_fail: 0
Rx DMA chan: pad_alloc_fail: 0
Rx DMA chan: runt_receive_buf: 0
Rx DMA chan: runt_transmit_buf: 0
Rx DMA chan: empty_dequeue: 0
Rx DMA chan: busy_dequeue: 855
Rx DMA chan: good_dequeue: 454
Rx DMA chan: requeue: 0
Rx DMA chan: teardown_dequeue: 0
Tx DMA chan: head_enqueue: 5
Tx DMA chan: tail_enqueue: 0
Tx DMA chan: pad_enqueue: 0
Tx DMA chan: misqueued: 0
Tx DMA chan: desc_alloc_fail: 0
Tx DMA chan: pad_alloc_fail: 0
Tx DMA chan: runt_receive_buf: 0
Tx DMA chan: runt_transmit_buf: 2
Tx DMA chan: empty_dequeue: 5
Tx DMA chan: busy_dequeue: 0
Tx DMA chan: good_dequeue: 5
Tx DMA chan: requeue: 5
Tx DMA chan: teardown_dequeue: 0
root@am335x-evm:~#
Thank you.