This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Watchdog connection on the EVM



Hi,

please can someone confirm the watchdog connection from EVM816x_Schematics_revb.pdf works ok when enabled by SW5? Unfortunately I do not have the EVM board and I can't test it by myself. Thank you very  much.

- Robert

 

From tms320c6a8167 datasheet: WD_OUT - Drives H (during PORn reset) / Drives L (after PORn and Warm reset are deasserted and during Warm reset L)

The connection in schematic looks to me like a loop:

During POR the WD_OUT output goes H ... through U36 - output is L ... through U34 - output is L -> PORn = L => WD_OUT = H

Please correct me.

 

 

  • I also have this problem, right now, we donot consider to connect watchdog output to porz, but we still need figure out this problem, and I also notice that Ti did some modification on EVM board http://processors.wiki.ti.com/index.php/TI81XX_PSP_WDT_Driver_User_Guide,

    so my question is, when the WD_OUT pin  is pulled down as the modification, the porz can be asserted only when WD_OUT is high, is that reasonable, cause WD_OUT should active low when it is asserted(count overflow) ?   

  • Hi Kevin,

    There are two silicon bugs related to the WDT in DM816x device.

    http://www.ti.com/lit/er/sprz329d/sprz329d.pdf

    Advisory 2.1.65 -  Watchdog Timer (WDT): Watchdog Timer Generates Reset When Enabled For First Time After Power-On Reset
    Revisions Affected:  2.1, 2.0
    Advisory 1.1.37 - Watchdog Timer (WDT): Default Timeout Period of 2 ms is Too Short
    Revisions Affected:  1.1, 1.0
    BR
    Pavel