Part Number: AM5706
Hi,
My customer has evaluated the DDR throughput performance of AM5706 with the following condition combinations.
- Core operation clock (1GHz / 800MHz / 600MHz / 400MHz)
- DDR Bus width (32bit / 16bit)
- Cache configurations (Enabled L1 cache and L2 cache / Enabled L1 cache only / Cache disabled)
- Consecutive access / Random access
As a result, The difference of throughput between 32bit and 16bit was just a few percent.
Do you think that this result is a reasonable outcome ?
Or the difference should be bigger ? If so, is there something wrong configuration on 16bit usage or 32bit usage ?
Best regards,
Hideaki