This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where is the Kernel Source Tree in EZSDK?

I would like to build the updated Syslink module and library that came with 02_00_00_68_beta1, but I need to alter the Makefile to indicate where the Kernel Source Tree is located.  You cannot build Linux modules without this and I am not sure where it is.

Is this it:

/home/lholeva/ti-ezsdk_c6a816x-evm_5_00_00_56/psp/linux-2.6.34-psp04.00.00.07

or perhaps:

/home/lholeva/ti-ezsdk_c6a816x-evm_5_00_00_56/psp/linux-2.6.34-psp04.00.00.07/kernel

Or, am wasting my time pursuing this as I do not have the 04.00.00.10 linux kernel?  PSP 04.00.00.10 appears to be not yet released.

It appears that even with the alpha syslink I have the same issus as I need to build the archive, syslink.a, and that also needs to know where the kernel source tree is. 

I may of answered my own question.  I set the kernel source path to

/home/lholeva/ti-ezsdk_c6a816x-evm_5_00_00_56/psp/linux-2.6.34-psp04.00.00.07/kernel

and I was able to build the syslink library for syslink_02_00_00_56.  I was also able to upgrade IPC to the latest version, 1_22_05_27.

 

Lee Holeva