Part Number: TDA4VM
hi expert
when i build QNX+RTOS SDK8.1
i found $/PSDKRA/vision_apps/apps/concerto_a72.inc.mak add four line 130-133
The addition of these will cause link library errors
Required system library libvx_tiovx_tests.a Required system library libvx_conformance_tests.a Required system library libvx_conformance_engine.a Required system library libvx_conformance_tests_testmodule.a Required system library libvx_kernels_hwa_tests.a Required system library libvx_tiovx_tidl_tests.a /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_awbalg /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_dcc collect2: error: ld returned 1 exit status concerto/finale.mak:212: recipe for target '/home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_single_cam.out' failed make[1]: [/home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_single_cam.out] Error 1 (ignored) Required system library libvx_kernels_test_kernels.a Required system library libvx_target_kernels_source_sink.a Required system library libvx_kernels_test_kernels_tests.a Linking /home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_viss.out Linking /home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_conformance.out Linking /home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_tutorial.out Linking /home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/libtivision_apps.so /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_awbalg /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_dcc collect2: error: ld returned 1 exit status concerto/finale.mak:212: recipe for target '/home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_viss.out' failed make[1]: [/home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_viss.out] Error 1 (ignored) Linking /home/tda4/TDA4_SDK8.1/PSDKRA/vision_apps/out/J7/A72/QNX/release/vx_app_sfm.out /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_awbalg /home/tda4/qnx710/host/linux/x86_64/usr/bin/aarch64-unknown-nto-qnx7.1.0-ld: cannot find -lti_imaging_dcc
Cancel these four lines to compile and pass
Is this change correct?
How to change if it is incorrect
What are the functions of the four added libraries