Hi,
We want to acquire two 8MP camera images. Modify the csi rate to CSIRX_LANE_BAND_SPEED_2250_TO_2500_MBPS,but no video stream and data. Is there any reason for this problem? Can csi lane speed be set CSIRX_LANE_BAND_SPEED_2250_TO_2500_MBPS?
At the same time, we did the following experiments,
one 8MP camera, csi rate to CSIRX_LANE_BAND_SPEED_1350_TO_1500_MBPS, Can be displayed normally(use run_app_single_cam.sh).
two 8MP camera, csi rate to CSIRX_LANE_BAND_SPEED_1350_TO_1500_MBPS, Image is floral or abnormal, have video stream(use run_app_single_cam.sh to select one of the cameras).
one 8MP camera, csi rate to CSIRX_LANE_BAND_SPEED_2250_TO_2500_MBPS, no video stream and data(use run_app_single_cam.sh).
The configuration is as follows,
static IssSensor_CreateParams ecarx_8MPCreatePrms = {
8MP_UYVY, /*sensor name*/
0x6, /*i2cInstId*/
{0, 0, 0, 0, 0, 0, 0, 0}, /*i2cAddrSensor*/
{0, 0, 0, 0, 0, 0, 0, 0}, /*i2cAddrSer*/
/*IssSensor_Info*/
{
{
8MP_OUT_WIDTH, /*width*/
8MP_OUT_HEIGHT, /*height*/
1, /*num_exposures*/
vx_false_e, /*line_interleaved*/
{
{VX_DF_IMAGE_UYVY, 7}, /*dataFormat and MSB [0]*/
},
0, /*meta_height_before*/
0, /*meta_height_after*/
},
ISS_SENSOR_8MP_FEATURES, /*features*/
ALGORITHMS_ISS_AEWB_MODE_NONE, /*aewbMode*/
30, /*fps*/
4, /*numDataLanes*/
{1, 2, 3, 4}, /*dataLanesMap*/
{0, 0, 0, 0}, /*dataLanesPolarity*/
//CSIRX_LANE_BAND_SPEED_2250_TO_2500_MBPS, //Cannot display normally, no video stream
CSIRX_LANE_BAND_SPEED_1350_TO_1500_MBPS, //Can be displayed normally
},
4, /*numChan*/
800, /*dccId*/
};