Experts:
I want to use MCU timer0 to capture PWM from PAD_E22. So I program codes and run on MCU1_0,
accordign to <SPRUIL1B-J721E DRA829TDA4VM-TRM>5.1.2.4, 12.10.3.4.6 and 12.10.3.5.2.3.
Input 500Hz, VPP=3V square wave to PAD_E22. PAD_E22 remains low after the program is running.
If PAD_E22 is configured as GPIO input, the injected square wave is detected at PAD_E22.
what are the reasons?
Registers' value:
TIOCP_CFG CBASS0 @0x40400010 A
IRQ_EOI @0x40400020 0
IRQSTATUS_RAW @0x40400024 0
IRQSTATUS @0x40400028 0
IRQWAKEEN @0x40400034 0
TCLR @0x40400038 432B
TCRR @0x4040003C 73A24
TLDR @0x40400040 0
TTGR @0x40400044 FFFFFFFF
TWPS @0x40400048 0
TMAR @0x4040004C 0
TCAR1 @0x40400050 0
TSICR @0x40400054 4
TCAR2 @0x40400058 0
TPIR @0x4040005C 0
TNIR @0x40400060 0
TCVR @0x40400064 0
TOCR @0x40400068 0
TOWR @0x4040006C 0
CTRLMMR_MCU_TIMER0_CLKSEL @0x40F08100 0
CTRLMMR_MCU_TIMER0_CTRL @0x40F04200 0
CTRLMMR_MCU_TIMERIO0_CTRL @0x40F04280 F
CTRLMMR_WKUP_PADCONFIG21 @0x4301C054 50002