Part Number: TDA4VM
hi:
our product has 4 2M camera and we want them work in 6 seconds.
The sdk is linux + rtos. version is 8.1
I think there's 3 ways to meet the requirement
1. cpus in Main domain enter into standby mode, such as WFI.
in this case, How much power consumption?
2. cpus in Main domain enter into low power mode. Power to main domain is turned OFF.
in this case, does the sdk8.1 support now? Is there any roadmap for the feature?
3. TDA4 do cold boot as soon as possible
is this any test data about cold boot? after remove all debug feature, such as uart and so on.
Thanks