This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Use NDK to send out packet through PHY

Guru* 95265 points

Dear all,

In MCSDK 1.0 or 2.0 package, do you have any sample test code using NDK to send packet to the network?

Regards, Eric

 

 

 

  • Eric,

    Yes, there are example projects.  I see the following info from a similar forum post:

     

    Peter, Santosh,

    BIOS MCSDK 1.0 actually includes NDK example projects. For C6474, then can be found in:

    C:\Program Files\Texas Instruments\mcsdk_1_00_00_08\packages\ti\platform\nimu\test\evm6474l

    Besides C6474, the other two C64x+ devices supported are C6472 and C6457.

    Hope this helps,

    Raj

     

    You can find the full post here:

    http://e2e.ti.com/support/embedded/f/355/p/87205/301324.aspx#301324

     

    Steve