This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: MCU CAN0 can not work

Part Number: TDA4VM

Hi 

We use socket can driver under Linux to drive MCU can0, hardware pin is D29 and C29.This is the same as SK board.

we build one sd card image.

1,SK board,the image can let mcu can0 work normally.

2,also the same sd card image,insert our board,mcu can0 can not work normally,can test from PC,can not receive right frame.act as eror frame.

To hardware,we just modify the can transceiver,from TCAN1046 to TJA1044.

Besides,we also do below experiment:

Connect SD board TDA4 TXD and RXD to transceiver (on our own board), we can receive right can message from PC.(by the way,we use the same one sd card image)

So we doublt whether there is some difference between our board's TDA4 and SK board's TDA4 SOC.

But we check our bom,SOC is the same as SK's board.

Please help give some opinion how to debug this issue

Thanks