Part Number: TDA4VM
I am getting following error let me know the solution
1041.751697 s: VX_ZONE_INIT:[app_create_graph:1066] minval init: 1041.751699 s: VX_ZONE_INIT:[app_create_graph:1068]
maxval init: 1041.751710 s: VX_ZONE_INIT:[app_create_graph:1070]
maxval count init: 1042.020101 s: VX_ZONE_ERROR:[ownContextSendCmd:782] Command ack message returned failure cmd_status: -7
1042.020126 s: VX_ZONE_ERROR:[ownContextSendCmd:818] tivxEventWait() failed.
1042.020137 s: VX_ZONE_ERROR:[ownNodeKernelInit:526] Target kernel, TIVX_CMD_NODE_CREATE failed
1042.020147 s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Please be sure the target callbacks have been registered for this core
1042.020157 s: VX_ZONE_ERROR:[ownNodeKernelInit:528] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
1042.020343 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 6, kernel com.ti.img_proc.od.fetch.box.detections ... failed !!!
1042.020375 s: VX_ZONE_ERROR:[vxVerifyGraph:2013] Node kernel init failed
1042.020383 s: VX_ZONE_ERROR:[vxVerifyGraph:2067] Graph verify failed
1042.126607 s: ISS: De-initializing sensor [IMX390-UB953_D3] ... !!!
1042.126776 s: ISS: De-initializing sensor [IMX390-UB953_D3] ... Done !!!
1042.127498 s: VX_ZONE_ERROR:[ownReleaseReferenceInt:307] Invalid reference
Thanks & Regards,
Vel