Other Parts Discussed in Thread: TMDSHSECDOCK
Hello!
I am currently working with a TMS320F28379D on a TMDSHSECDOCK controlCard and am working with the Built in Self Tests (BIST). I have loaded the 'f2837xd_test_application onto the device and when running the code I receive the terminal message 'TEST FAIL: ADC/DAC 12-Bit Test!'.
Just curious as to why this is? Looking at the code it seems to be doing a simple comparison between the ADC and DAC values (as expected) and I have ADC-B0 connected to 3.3V per the C2000 SafeTI
Diagnostic Library Self-Test Application User Guide for the reference voltage.
Will keep plugging away just looking for any insight!
Best Regards,
Chris