This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: Fusion Board Configuration File

Part Number: TDA4VM-Q1
Other Parts Discussed in Thread: TDA4VM, DS90UB960-Q1, DS90UB953-Q1

Hi team,

  1. DS90UB953-Q1 as Ser chip, and paired with Des chip DS90UB960-Q1 on TDA4VM fusion board - any initialization configuration file? 
  2. Is below synchronous mode is compatible with EVM577PFUSION board? 

  • Hi PY,

    1. Refer to any of the sensor driver's serdes configuration. Example: ti-processor-sdk-rtos-j721e-evm-08_00_00_12/imaging/sensor_drv/src/imx390/imx390_serdes_config.h or any other ti-processor-sdk-rtos-j721e-evm-08_00_00_12/imaging/sensor_drv/src/SENSOR_NAME/SENSOR_NAME_serdes_config.h

    2. Yes it is possible to use synchronous mode with Fusion Board. Make sure Deserializer register 0x58 is programmed to 0x5E on the Deserializer and Serializer register 0x03 is 0x10 if they are not strapped to be in Sync mode.