Part Number: TMDSEVM572X
Hi,
I have an application which i'm building using cmake.When i run cmake it looks for few dependant libraries.Below are the details of it:
Found OpenSSL: /usr/lib/libcrypto.so (found version "1.1.1b")
-- Found PCAP: /usr/lib/libpcap.so
-- Could NOT find MARIADB (missing: MARIADB_LIBRARY MARIADB_INCLUDE_DIR)
-- Found SQLite3: /usr/lib/libsqlite3.so (found version "3.23.1")
-- Found Protobuf: /usr/lib/libprotobuf.so;-lpthread;-lpthread (found version "3.6.1")
-- Found Eigen3: /usr/include/eigen3 (Required is at least version "2.91.0")
-- Found FMT: /usr/lib/libfmt.so
-- Boost version: 1.68.0
-- Found the following Boost libraries:
-- thread
-- system
-- filesystem
-- chrono
-- date_time
-- atomic
-- Found Perl: /usr/bin/perl (found version "5.24.4")
But the mariadb library is missing in the target platform .I also installed the mariadb libraries using the recipes-dbs provided by meta-openembedded. Only libmysqlclient.so is installed but i also need libmariadb.so.
- Details of platform used:
Platform : TMDSEVM572X
SDK used : PROCESSOR-SDK-LINUX-RT-AM57X
I used the same steps as given in this link software-dl.ti.com/.../Overview_Building_the_SDK.html
Request you suggest the suitable solution at the earliest
Thanks in advance.