Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517EVM Starting kernel fails

Other Parts Discussed in Thread: AM3517

Hi,

 

I compiled new linux kernel from "AM35x-OMAP35x-PSP-SDK-03.00.00.05.tar", with new modules (ie: for switch SMSC LAN 9311 on LOGIC PD board).

I compiled u-boot to have u-boot.bin and kernel to have uImage, and copied both on SDcard.

When I boot the board with card, X-Loader and U-Boot work, read linux Image but stop after "Starting kernel...", there is no "uncompressing linux..................." like with original version :


Texas Instruments X-Loader 1.46 (Jan 22 2011 - 01:46:00)
Starting X-loader on MMC
Reading boot sector

214940 Bytes Read from MMC
Starting OS Bootloader from MMC...
Starting OS Bootloader...


U-Boot 2009.11 (Mar 19 2010 - 19:46:20)

OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz
AM3517EVM Board + LPDDR/NAND
I2C:   ready
DRAM:  256 MB
NAND:  512 MiB
*** Warning - bad CRC or NAND, using default environment

In:    serial
Out:   serial
Err:   serial
Die ID #0736000100000000015da3960e01f01d
Net:   davinci_emac_initialize
Ethernet PHY: GENERIC @ 0x00
DaVinci EMAC
Hit any key to stop autoboot:  0
mmc1 is available
reading boot.scr
Invalid FAT entry

** Unable to read "boot.scr" from mmc 0:1 **
reading uImage

3114428 bytes read
Booting from mmc ...
## Booting kernel from Legacy Image at 82000000 ...
   Image Name:   Linux_perso
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3114364 Bytes =  3 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

 

I used mkimage to configure Load Address and Entry Address with same values as example but nothing.

Someboby can help me ?

Thanks

  • Hi,

         Can you post the set environment variables?

          Typing "printenv" in the u-boot prompt provides all the necessary information.

     

    Regards,

    N.S.SriHarsha

  • Hi,

    Sorry for this oversight...

    Texas Instruments X-Loader 1.46 (Jan 22 2011 - 01:46:00)
    Starting X-loader on MMC
    Reading boot sector

    214940 Bytes Read from MMC
    Starting OS Bootloader from MMC...
    Starting OS Bootloader...


    U-Boot 2009.11 (Mar 19 2010 - 19:46:20)

    OMAP34xx/35xx-GP ES1.0, CPU-OPP2 L3-165MHz
    AM3517EVM Board + LPDDR/NAND
    I2C:   ready
    DRAM:  256 MB
    NAND:  512 MiB
    *** Warning - bad CRC or NAND, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Die ID #0736000100000000015da3960e01f01d
    Net:   davinci_emac_initialize
    Ethernet PHY: GENERIC @ 0x00
    DaVinci EMAC
    Hit any key to stop autoboot:  0
    AM3517_EVM # printenv
    bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
    bootdelay=10
    baudrate=115200
    bootfile=uImage
    loadaddr=0x82000000
    console=ttyS2,115200n8
    mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
    nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2
    loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
    bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
    loaduimage=fatload mmc 0 ${loadaddr} uImage
    mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
    nandboot=echo Booting from nand ...; run nandargs; nand read ${loadaddr} 280000 400000; bootm ${loadaddr}
    stdin=serial
    stdout=serial
    stderr=serial
    dieid#=0736000100000000015da3960e01f01d
    ethact=DaVinci EMAC

    Environment size: 859/131068 bytes
    AM3517_EVM #

     

    Regards,

     

    JF_Sor

  • I've seen that happen when the machine type enumeration is different between the U-Boot image and Linux kernel image. The machine type is in generated file called mach-types.h. U-Boot just silently stops the kernel boot without a message.

    This might not be the source of your problem though.

  • Hi,

            The boot arguments look fine, i reckon it is something to do with the kernel image. Can you enable earlyprintk in the kernel -> menuconfig -> kernel hacking -> kernel low level debugging functions and post the log.

     

    Regards,

    N.S.SriHarsha

  • Hi,

    there was a bad configuration of uBoot and mkImage tools.

    It's good for me, thanks for your answers.

    Regards,

    JF_Sor