This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using CSL EDMA3 with interrupts

Hi,

I am trying to configure a edma3 transfer with a transfer completion function.

I found an example for such code but I receive an error in the following line:

hIntc = CSL_intcOpen (&intcObj, CSL_INTC_EVENTID_EDMA3CC_GINT,&vectId , NULL);

Error:  identifier "CSL_INTC_EVENTID_EDMA3CC_GINT" is undefined.
To my understaning CSL_INTC_EVENTID_EDMA3CC_GINT should be the relevent event number.
In this doc: http://focus.ti.com/lit/ds/symlink/tms320c6678.pdf  there is a list of all the events but  which is the correct event number I need to use?
(my configurations are for a C6678 simulation using CCS 5.0.2 and bios mcsdk 2.0)
In the saem document it sais:
"For more details on the
INTC features, please refer to the Interrupt Controller (INTC) for KeyStone Devices User Guide (literature number
SPRUGW4)." But the link is broken and the INTC user guide is nowhere to be found.
thank you for your help.

  • Ya,

    This user guide has not been published yet, it should be soon.  That said, the UG is not going to have descriptions of the events and the event numbers which are unique to the Keystone devices.  This information is in the Data Manual you're using. 

    I'm going to ask someone from the SW support side to help out on this.

    -Chad

  • Hi,

    I am now using the MCSDK2.0 Beta for C6678 and I have met the same problem!

    My question is, will  MCSDK2.0 adds more examples about edma interrupts, just as C6747 does  in MCSDK1.0? I am waiting for it eagarly!

    Best regards!

    Johnny

  • That is what worked for me (I took the code from the CSL examples, probably some lines are unnecessary)

     

    CSL_Edma3Handle                 hModule;

    CSL_Edma3Obj                    edmaObj;

    CSL_Edma3ParamHandle            hParam;

    CSL_Edma3ChannelObj             chObj;

    CSL_Edma3CmdIntr                regionIntr;

    CSL_Edma3ChannelHandle          hChannel;

    CSL_Edma3ParamSetup             myParamSetup;

    CSL_Edma3Context                context;

    CSL_Edma3ChannelAttr            chAttr;

    CSL_Status                      status;

     

    CSL_IntcObj                 intcObj;

    CSL_IntcGlobalEnableState   state;

    CSL_IntcContext             intcContext;

    CSL_Status                  intStat;

    CSL_IntcParam               vectId;

    CSL_IntcEventHandlerRecord  EventRecord;

    CSL_IntcHandle hIntc;

    CSL_IntcEventHandlerRecord      EventHandler[30];

    EdmaTccHandler TccHandlerTable[64];

    CSL_IntcRegsOvly CSL_IntcReg;

    CSL_CPINTC_Handle hnd;

    if (CSL_edma3Init(&context) != CSL_SOK)

    {

    printf ("Error: EDMA module initialization failed\n");

    return -1;

    }

    /* Open the EDMA Module using the provided instance number */

    hModule = CSL_edma3Open(&edmaObj, instNum, NULL, &status);

    if ( (hModule == NULL) || (status != CSL_SOK))

    {

    printf ("Error: EDMA module open failed\n");

    return -1;

    }

     

    /* Channel open */

    chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;

    chAttr.chaNum    = channelNum;

    hChannel = CSL_edma3ChannelOpen(&chObj, instNum, &chAttr, &status);

    if ((hChannel == NULL) || (status != CSL_SOK))

    {

    printf ("Error: Unable to open EDMA Channel:%d\n", channelNum);

    return -1;

    }

     

    /* Change Channel Default queue setup from 0 to 3  */

    if (CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3) != CSL_SOK)

    {

    printf ("Error: EDMA channel setup queue failed\n");

    return -1;

    }

     

    /* Map the DMA Channel to PARAM Block 2. */

    CSL_edma3MapDMAChannelToParamBlock (hModule, channelNum, 2);

     

    /* Obtain a handle to parameter set 2 */

    hParam = CSL_edma3GetParamHandle(hChannel, 2, &status);

    if (hParam == NULL)

    {

    printf ("Error: EDMA Get Parameter Entry failed for 1.\n");

    return -1;

    }

     

    /* Setup the parameter entry parameters (Ping buffer) */

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \

    CSL_EDMA3_TCCH_DIS, \

    CSL_EDMA3_ITCINT_EN, \

    CSL_EDMA3_TCINT_EN, \

    TCC_NUM, CSL_EDMA3_TCC_NORMAL,\

    CSL_EDMA3_FIFOWIDTH_NONE, \

    CSL_EDMA3_STATIC_DIS, \

    CSL_EDMA3_SYNC_A, \

    CSL_EDMA3_ADDRMODE_INCR, \

    CSL_EDMA3_ADDRMODE_INCR );

    myParamSetup.srcAddr    = (Uint32)srcBuff1;

    myParamSetup.aCntbCnt   = CSL_EDMA3_CNT_MAKE(N,1);

    myParamSetup.dstAddr    = (Uint32)dstBuff1;

    myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);

    myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);

    myParamSetup.cCnt = 1;

     

    /* Param setup */

    if (CSL_edma3ParamSetup(hParam,&myParamSetup) != CSL_SOK)

    {

    printf ("Error: EDMA Parameter Entry Setup failed\n");

    return -1;

    }

    regionIntr.region = CSL_EDMA3_REGION_GLOBAL;

    regionIntr.intr   = 0;

    regionIntr.intrh  = 0x0;

    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&regionIntr);

     

     

    hnd = CSL_CPINTC_open(0);

    if (hnd == 0)

    {

    printf ("Error: Unable to open CPINTC-0\n");

    return -1;

    }

     

    /* Disable all host interrupts. */

    CSL_CPINTC_disableAllHostInterrupt(hnd);

     

    /* Configure no nesting support in the CPINTC Module. */

    CSL_CPINTC_setNestingMode (hnd, CPINTC_NO_NESTING);

     

    /* Map System Interrupt 36 (EDMACC GINT) to channel 3 */

    CSL_CPINTC_mapSystemIntrToChannel (hnd, 36 , 3);

     

    /* Enable system interrupt 36 */

    CSL_CPINTC_enableSysInterrupt (hnd, 36);

     

    /* We enable host interrupts. */

    CSL_CPINTC_enableHostInterrupt (hnd, 3);

     

    /* Enable all host interrupts also. */

    CSL_CPINTC_enableAllHostInterrupt(hnd);

     

    intcContext.eventhandlerRecord = EventHandler;

    intcContext.numEvtEntries      = 10;

    /* Initiate INTC module */

    if (CSL_intcInit(&intcContext) != CSL_SOK)

    {

    printf("Error: GEM-INTC initialization failed\n");

    return -1;

    }

     

    /* Enable NMIs */

    if (CSL_intcGlobalNmiEnable() != CSL_SOK)

    {

    printf("Error: GEM-INTC global NMI enable failed\n");

    return -1;

    }

     

    /* Enable global interrupts */

    if (CSL_intcGlobalEnable(&state) != CSL_SOK)

    {

    printf ("Error: GEM-INTC global enable failed\n");

    return -1;

    }

     

    /* Open the INTC Module for Vector ID: 4 and Event ID: 63(INTC0_OUT3)*/

    vectId = CSL_INTC_VECTID_4;

    hIntc = CSL_intcOpen (&intcObj, 63, &vectId , NULL);

    if (hIntc == NULL)

    {

    printf("Error: GEM-INTC Open failed\n");

    return -1;

    }

     

    /* Register an call-back handler which is invoked when the event occurs. */

    EventRecord.handler = &eventHandler;

    EventRecord.arg = 0;

    if (CSL_intcPlugEventHandler(hIntc,&EventRecord) != CSL_SOK)

    {

    printf("Error: GEM-INTC Plug event handler failed\n");

    return -1;

    }

     

    /* Enabling the events. */

    if (CSL_intcHwControl(hIntc,CSL_INTC_CMD_EVTENABLE, NULL) != CSL_SOK)

    {

    printf("Error: GEM-INTC CSL_INTC_CMD_EVTENABLE command failed\n");

    return -1;

    }

     

    /* Trigger channel */

    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

  • The event mapping is in the data manual. I though the INC UG already got published. I will verify that, or else will attach to this forum.

     

    Thanks,

    Arun.

  • Also where did you get that event ID you mentioned in your first post. I didnot see anywhere in the CSL.

     

    Thanks,

    Arun.

  • I got it from the example that came with the CSL

  • Hi,

    Please could you post the whole example that you talked about.

    I didn't find it in CSL.  The only example I found is located in:

    \pdk_C6678_1_0_0_9_beta2\packages\ti\csl\example\edma\edma_test.c, and it doesn't work

    also this example is very different from the code you post on may 5th

    Thanks in advance.

    Shmulik