Part Number: AM6442
Other Parts Discussed in Thread: TPS745
Our customer is designing a prototype board with the AM6442 SR1.0 and powering the AM6442 + DDR memory with the single PMIC solution. And I have a few questions about the powering.
The power connections are as follows.

The following application note was referenced for the single PMIC solution.
Powering the AM64xx With the LP8733xx PMIC
www.ti.com/.../slvaes0.pdf
Figure 1. Powering AM64x With LP8733xx │DDR4 Memory
Can the GPO2 pin on the LP873364 be directly connected to the EN pin on the TPS6282x and the EN pin on the TPS745?
The output low level voltage (VOL) of the GPO2 pin on the LP873364 is 0.4V (MAX), but the input low level threshold voltage (VL) of the EN pin on the TPS6282x is 0.4V (MAX), and the input low level threshold voltage (VEN(LO)) of the EN pin on the TPS745 is 0.3V (MAX).
The power-up/down sequence in the power connections is as follows.

The following document was referenced for the power-up/down sequence of the LP873364.
LP873364 Technical Reference Manual
www.ti.com/.../snvu810.pdf
Figure 3-1. LP873364 Power-up and Power Down Sequence
Can the power-down sequence of the LP873364 meet the power-down sequence of the AM64x requirements?
VDD_CORE on AM64x is not allowed to be ramped down before other power supply inputs.

Best regards,
Daisuke