This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5505 RTC Write Access



I am using the 32KHz RTC clock with the PLL to generate the SYSCLK.  When  I run the example CSL_RTC_Example_Out project, I notice that none of the writes to the RTC registers actually take place.

Is it possible to write to the RTC registers when using the 32KHz clock for SYSCLK? Or do I need to do something special to make that happen?

I am running version C55XCSL-LOWPOWER-2.10.00.00 and CCS 4.2.3.00004

Thanks in advance!